Skip to main content
FTajb.1
Visitor II
December 11, 2019
Question

Using hardware based wake-up in combination with the automatic antenna tuning feature is not recommended. I like to use both what should I do. And what is the card read range with this device

..

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    December 11, 2019

    I guess you'd read all the docs, review all the code, and then own the dev/debug task to make it ​work.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Brian TIDAL
    ST Technical Moderator
    December 12, 2019

    Hi,

    can you provide more information about your request:

    • which ST25 device, what is your HW setup, custom board or ST board, etc.
    • FW setup, etc
    • what is your application

    Thanks

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.