Skip to main content
Associate II
June 8, 2025
Solved

Understanding and Using UNTRACEABLE Mode in ST25TV Tags

Hello ST Community,

I've been exploring STEVAL-25R200A dev kit using the X-CUBE-NFC10 package-based sample application. Currently, I am testing the UNTRACEABLE mode feature in the ST25TV tag. However, I’m noticing some unexpected behavior and would love to get help and support.

In my case UNTR_CMD = 1b and as per the Table 70 of the specifications, the device (ST25TV tag) should boot in UNTRACEABLE state irrespective of any UNTR_DFT value, and in this state, it should only respond to Get Random Number and Present Password commands. However, in my testing, I’ve found that when UNTR_CMD = 1b and UNTR_DFT = 0, the tag responds to every command which it should not.

This makes me wonder if I’ve understood the UNTRACEABLE mode correctly or not.

 

Regards,
Tanuj

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
June 10, 2025

Hi Tanuj,

make sure to check the Response_flags of the ToggleUntraceable response. It is likely that Error_flag equals 1 due to  something wrong in the ToggleUntraceable request. Make sure to follow section 5.1.3 Password encryption when building the unique valid Password_data value in the ToggleUntraceable command.

Note: the untraceable mode can be exercised with the ST25PC-NFC. Start the ST25R200 Eval Gui and click on the ST25PC-NFC icon:

BrianTIDAL_0-1749544239508.png

Once running the ST25PC-NFC, go to the Untraceable mode menu.

BrianTIDAL_1-1749544364265.png

Then, you can toggle the untraceable mode and check its behavior.

BrianTIDAL_2-1749544431713.png

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
June 10, 2025

Hi Tanuj,

make sure to check the Response_flags of the ToggleUntraceable response. It is likely that Error_flag equals 1 due to  something wrong in the ToggleUntraceable request. Make sure to follow section 5.1.3 Password encryption when building the unique valid Password_data value in the ToggleUntraceable command.

Note: the untraceable mode can be exercised with the ST25PC-NFC. Start the ST25R200 Eval Gui and click on the ST25PC-NFC icon:

BrianTIDAL_0-1749544239508.png

Once running the ST25PC-NFC, go to the Untraceable mode menu.

BrianTIDAL_1-1749544364265.png

Then, you can toggle the untraceable mode and check its behavior.

BrianTIDAL_2-1749544431713.png

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.