Skip to main content
Associate II
March 3, 2025
Solved

Trouble with NUCLEO-L053R8 and X-NUCLEO-NFC06A1

Hello!

I am using ST25R3916 (X-NUCLEO-NFC06A1) and RFAL Library V3.0.1. When working with STM32L4RGT3 (NUCLEO-L476RG) everything works fine, but if I use STM32L053R8 (NUCLEO-L053R8) functions rfalNfcaPollerFullCollisionResolution() and rfalISO14443ATransceiveAnticollisionFrame() regardless of MCU frequency and stack size settings all the time return RFAL_ERR_FRAMING error.

What could be the reason for this behavior depending on the MCU?

STM32L053R8 (NUCLEO-L053R8) together with ST25R3911 (X-NUCLEO-NFC05A1) works fine, but when connected to ST25R3916 (X-NUCLEO-NFC06A1) it gives this error..

Best regards, Rob.

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
March 3, 2025

Hi Rob,

 

I've build the polling application based on NUCLEO-L053R8 and I do not face any issues. I've attached the ioc file for reference.

Can you confirm that the sample NUCLEO-L476RG application uses RFAL_ANALOG_CONFIG_CUSTOM + analogConfigTbl_NFC06A1.c? Can you confirm that the generated NUCLEO-L053R8 application also uses RFAL_ANALOG_CONFIG_CUSTOM (inrfal_defConfig.h) + analogConfigTbl_NFC06A1.c?

Can you confirm your application uses X-CUBE-NFC6 v3.1.0?

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Brian TIDAL
ST Technical Moderator
March 3, 2025

Hi Rob,

have you based your application on X-CUBE-NFC6 package or do you have ported the RFAL 3.0.1 by yourself or have you used the ST25 embedded NFC library?

How are managed the analog config on the various platform (NUCLEO-L476RG and NUCLEO-L053R8)? do you use custom analog config?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Rob_TalorAuthor
Associate II
March 3, 2025

I created my application in STM32CubeMX and using the Software Packs Conponent Selector I included the STMicroelectronics.X-CUBE-NFC6 pack in accordance with the manual "Getting started with the X-CUBE-NFC6 high performance HF reader/NFC initiator. IC software expansion for STM32Cube".
Is used the default Analog configuration for the ST25R3916. Dynamic analog configuration or user analog configuration are not used.

Maybe there are other ways of correct porting of X-CUBE-NFC6 for NUCLEO-L053R8?

For ST25R3916 (X-NUCLEO-NFC06A1) I found sample applications only for NUCLEO-L476RG and NUCLEO-G0B1RE, but there are no sample applications for NUCLEO-L053R8.

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
March 3, 2025

Hi Rob,

 

I've build the polling application based on NUCLEO-L053R8 and I do not face any issues. I've attached the ioc file for reference.

Can you confirm that the sample NUCLEO-L476RG application uses RFAL_ANALOG_CONFIG_CUSTOM + analogConfigTbl_NFC06A1.c? Can you confirm that the generated NUCLEO-L053R8 application also uses RFAL_ANALOG_CONFIG_CUSTOM (inrfal_defConfig.h) + analogConfigTbl_NFC06A1.c?

Can you confirm your application uses X-CUBE-NFC6 v3.1.0?

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.