Skip to main content
Ivanova Anastasiia
Associate
June 19, 2017
Solved

The maximum range CR95HF

Posted on June 19, 2017 at 07:34

Hello, everybody. What is the maximum range one's achieved with CR95HF? I mean the proximity range. Is is possible to achieve 10cm and more with it? Could we achieve the better distance with ST95 for example?

    This topic has been closed for replies.
    Peter Boringer
    Peter BoringerBest answer
    Visitor II
    January 15, 2018
    Posted on January 15, 2018 at 14:04

    Hello Anastasiia,

    It depend on the protocol you are using and the antenna properties your are designing.

    If you speak about proximity 14443 protocol with the Discovery kit for CR95HF Reader you can reach 4 cm.

    If you are in Viccinity 15693 protocol with the same kit you can reach up to 7 cm

    But again this kit is a general purpose multi protocol setup and can be specifically trimmed and adapted.

    I can suggest you for better performances to use a ST25R3911 demonstartor board.

    Regards

    1 reply

    Peter Boringer
    Peter BoringerBest answer
    Visitor II
    January 15, 2018
    Posted on January 15, 2018 at 14:04

    Hello Anastasiia,

    It depend on the protocol you are using and the antenna properties your are designing.

    If you speak about proximity 14443 protocol with the Discovery kit for CR95HF Reader you can reach 4 cm.

    If you are in Viccinity 15693 protocol with the same kit you can reach up to 7 cm

    But again this kit is a general purpose multi protocol setup and can be specifically trimmed and adapted.

    I can suggest you for better performances to use a ST25R3911 demonstartor board.

    Regards