Skip to main content
Cmath.1
Associate
March 9, 2020
Solved

TAG SVT25 SERIES: Please kindly confirm the RFID reading distance is around 1 meter..? If so , which can of RFID reader equipment are suitable on a storage warehouse?

  • March 9, 2020
  • 1 reply
  • 574 views

..

    This topic has been closed for replies.
    Best answer by Berenice BENVEGUDA

    Hello,

    First of thanks for you interest in ST25 products !

    The ST25TV is a type 5 NFC certified tag, based on ISO15693 RFID protocol. The rule of thumbs for ISO15693 is the range is approximately the size of the reader antenna. So with NFC smartphones, the type5 tags operate within less than 10cm. And reaching 1m range is possible using a high power RFID reader (portal type, from companies like FEIG) and proper tag antenna design. Please contact your local ST sales office if you need any help.

    Best Regards,

    BB

    1 reply

    Berenice BENVEGUDA
    ST Technical Moderator
    March 26, 2020

    Hello,

    First of thanks for you interest in ST25 products !

    The ST25TV is a type 5 NFC certified tag, based on ISO15693 RFID protocol. The rule of thumbs for ISO15693 is the range is approximately the size of the reader antenna. So with NFC smartphones, the type5 tags operate within less than 10cm. And reaching 1m range is possible using a high power RFID reader (portal type, from companies like FEIG) and proper tag antenna design. Please contact your local ST sales office if you need any help.

    Best Regards,

    BB