Skip to main content
DRich.1
Associate II
Oct 30, 2019 8:55 AM UTC
Solved

Succesfull SendReceive write command to Mifare Ultralight EV1 sometimes responds with succes code, sometimes with error code

Error - 8700 : Frame wait time out OR no tag

Even though a writeis succesfull, I will at one time get this error code back (this is the answer of the SendReceive, the result of SendReceive itself is errorcode '4 ' which stands for Communication Error), and another time a succes code. I know the write is succesfull because in the next read I can read the value that was written.

The problem with this is that I cannot check whether or not the write was succesfull and then try again, because this may put me in an infinite loop.

What can be the cause of this?

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Nov 4, 2019 9:57 AM UTC

    Hi,

    See the following post for this issue: https://community.st.com/s/question/0D50X0000AFqKjkSQF/why-does-my-cr95hf-respond-with-0x87-timeout-or-no-tag-after-successfully-writing-to-a-ntag216-nfc-forum-type-2-compliant-tag

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    1 reply

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Nov 4, 2019 9:57 AM UTC
    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.