Skip to main content
Associate II
October 26, 2023
Solved

stream mode configuration of the ST25R3911B

    我目前在使用的芯片是ST25R3911B,准备用于和我的另一个设备进行自定义协议的通信,但我在规格书内找不到关于“stream mode”的配置流程,想知道在什么地方可以找到流模式的参考例程。
    另外看到透明模式似乎也可以实现自定义协议的通信,但是规格书内提供的配置信息太少,能否提供透明模式的配置流程。

The following uses machine translation:
    I am currently using the chip ST25R3911B for custom protocol communication with another device of mine, but I cannot find the configuration flow for "stream mode" in the specification and would like to know where to find the reference routine for stream mode.
    In addition, it seems that the transparent mode can also realize the communication of the custom protocol, but the configuration information provided in the specification is too little, can you provide the configuration process of the transparent mode?
Best regards

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
December 5, 2023

Hi,

For stream mode just look at our RFAL where we use it for implementing NFC-V/ISO15693.

For Transparent mode please look around on the community. E.g.

Best Regards, Ulysses

 

2 replies

Jack_ChenAuthor
Associate II
December 5, 2023

通过简单的配置,目前已经可以使用stream mode发送数据,接收数据的功能还未实现。

Through simple configuration, the stream mode can be used to send data, and the function of receiving data has not been implemented.

Ulysses HERNIOSUS
ST Technical Moderator
December 5, 2023

Hi,

For stream mode just look at our RFAL where we use it for implementing NFC-V/ISO15693.

For Transparent mode please look around on the community. E.g.

Best Regards, Ulysses