Skip to main content
Egor Vasilyev
Associate II
April 16, 2018
Solved

STM32F407VG + M24SR

Posted on April 16, 2018 at 21:09

I'm trying to connect m24sr to stm32f407vgt.

I switch to I2C2, clocking from an external resonator at 8 MHz, SYSCLK 72 MHz, I use a converted library for Open107V. For stm32f107vc this code worked, but when switching to stm32f407 i2c does not work (most likely there is no response from m24sr and a timeout error occurs).

I've been puzzling for several days, I can not find the error.

Defines for i2c

&sharpdefine M24SR_SDA_PIN GPIO_Pin_11

&sharpdefine M24SR_SDA_PIN_SOURCE GPIO_PinSource11

&sharpdefine M24SR_SDA_PIN_PORT GPIOB

&sharpdefine M24SR_SCL_PIN GPIO_Pin_10

&sharpdefine M24SR_SCL_PIN_SOURCE GPIO_PinSource10

&sharpdefine M24SR_SCL_PIN_PORT GPIOB

&sharpdefine M24SR_GPO_PIN GPIO_Pin_15

&sharpdefine M24SR_GPO_PIN_PORT GPIOD

&sharpdefine M24SR_RFDIS_PIN GPIO_Pin_14

&sharpdefine M24SR_RFDIS_PIN_PORT GPIOD

&sharpif defined STM32F40_41xxx

&sharpdefine M24SR_GPIO_BLOCK_CLK (RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOD)

&sharpelse

&sharpdefine M24SR_GPIO_BLOCK_CLK (RCC_APB2Periph_GPIOB | RCC_AHB1Periph_GPIOD)

&sharpendif

/ * I2C config ---------------------------------------------- -------------------------------- * /

&sharpdefine M24SR_I2C I2C2

&sharpdefine M24SR_I2C_BLOCK_CLK RCC_APB1Periph_I2C2

&sharpdefine M24SR_I2C_CLOCKSPEED 400,000

The code itself

void M24SR_Init (void)

{

M24SR_I2CInit ();

M24SR_InitStructure ();

&sharpifdef I2C_GPO_SYNCHRO_ALLOWED

M24SR_KillSession ();

M24SR_RFConfig (0);

M24SR_ManageI2CGPO (I2C_ANSWER_READY);

M24SR_Deselect ();

 

&sharpendif / * I2C_GPO_SYNCHRO_ALLOWED * /

}

void M24SR_I2CInit (void)

{

GPIO_InitTypeDef GPIO_InitStructure;

I2C_InitTypeDef I2C_InitStructure;

  / * GPIO Periph clock enable * /

&sharpif defined STM32F40_41xxx

RCC_AHB1PeriphClockCmd (M24SR_GPIO_BLOCK_CLK, ENABLE);

&sharpelse

RCC_APB2PeriphClockCmd (RCC_APB2Periph_AFIO | M24SR_GPIO_BLOCK_CLK, ENABLE);

&sharpendif

  / * I2C Periph clock enable * /

  RCC_APB1PeriphClockCmd (M24SR_I2C_BLOCK_CLK, ENABLE);

  / * Configure I2C pins: SCL and SDA * /

  GPIO_InitStructure.GPIO_Pin = M24SR_SCL_PIN | M24SR_SDA_PIN;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

&sharpif defined STM32F40_41xxx

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

&sharpelse

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD;

&sharpendif

  GPIO_Init (M24SR_SDA_PIN_PORT, & GPIO_InitStructure);

&sharpif defined STM32F40_41xxx

/ * Connect I2C pins to AF * /

  GPIO_PinAFConfig (M24SR_SCL_PIN_PORT, M24SR_SCL_PIN_SOURCE, GPIO_AF_I2C2);

  GPIO_PinAFConfig (M24SR_SDA_PIN_PORT, M24SR_SDA_PIN_SOURCE, GPIO_AF_I2C2);

&sharpendif

  / * Configure GPIO for M24SR GPO as Input pull-up, used as Interuption comming from the M24SR * /

  GPIO_InitStructure.GPIO_Pin = M24SR_GPO_PIN;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

&sharpif defined STM32F40_41xxx

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

&sharpelse

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

&sharpendif

  GPIO_Init (M24SR_GPO_PIN_PORT, & GPIO_InitStructure);

/ * Configure GPIO for M24SR RF Disable signal * /

  GPIO_InitStructure.GPIO_Pin = M24SR_RFDIS_PIN;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

&sharpif defined STM32F40_41xxx

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

&sharpelse

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

&sharpendif

  GPIO_Init (M24SR_RFDIS_PIN_PORT, & GPIO_InitStructure);

  I2C_DeInit (M24SR_I2C);

  / * I2C Init * /

  I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

  I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

  I2C_InitStructure.I2C_OwnAddress1 = 0x00;

  I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

  I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

  I2C_InitStructure.I2C_ClockSpeed = M24SR_I2C_CLOCKSPEED;

  I2C_Init (M24SR_I2C, & I2C_InitStructure);

  / * I2C Init * /

  I2C_Cmd (M24SR_I2C, ENABLE);

}

static void M24SR_InitStructure (void)

{

/ * build the command * /

Command.Header.CLA = 0x00;

Command.Header.INS = 0x00;

/ * copy the offset * /

Command.Header.P1 = 0x00;

Command.Header.P2 = 0x00;

/ * copy the number of byte of the data field * /

Command.Body.LC = 0x00;

/ * copy the number of byte to read * /

Command.Body.LE = 0x00;

Command.Body.pData = DataBuffer;

}

uint16_t M24SR_KillSession (void)

{

uint8_t pBuffer [] = {M24SR_KILLSESSION};

int8_t status;

errchk (M24SR_SendI2Ccommand (0x01, pBuffer));

/ * insure no access will be done just after open session * /

/ * The only way here is to poll I2C to know when M24SR is ready * /

/ * GPO can not be used with KillSession command * /

errchk (M24SR_PollI2C ());

return M24SR_ACTION_COMPLETED;

Error:

/ * Send STOP Condition * /

  I2C_GenerateSTOP (M24SR_I2C, ENABLE);

return M24SR_ERROR_I2CTIMEOUT;

}

#stm32f407 #m24sr #i2c
This topic has been closed for replies.
Rene Lenerve
Rene LenerveBest answer
ST Employee
April 17, 2018
Posted on April 17, 2018 at 11:52

Hi Egor,

I do not see clearly an error that can explain your issue with the part of your code supplied. I see, however, some things that may be problematic.

Firstly, I would suggest that you do not use a comma separator for thousands in variable definitions or operations. (Could be problematic with compilers and regional settings).

#define M24SR_I2C_CLOCKSPEED 400000�?�?

Secondly, are you sure of your clock configuration, the clock tree is different between both MCUs.

Then, are you sure that signals from I²C are correctly send by the MCU when using the STM32F4 You can test in debug mode to see if the I²C is correctly configured and working or if you can directly check the electric signals.

May I also suggest you to use the syntax highlighter for your code example to ease the readability.

I hope this will help you in your debugging

.

Best Regards.

1 reply

Rene Lenerve
Rene LenerveBest answer
ST Employee
April 17, 2018
Posted on April 17, 2018 at 11:52

Hi Egor,

I do not see clearly an error that can explain your issue with the part of your code supplied. I see, however, some things that may be problematic.

Firstly, I would suggest that you do not use a comma separator for thousands in variable definitions or operations. (Could be problematic with compilers and regional settings).

#define M24SR_I2C_CLOCKSPEED 400000�?�?

Secondly, are you sure of your clock configuration, the clock tree is different between both MCUs.

Then, are you sure that signals from I²C are correctly send by the MCU when using the STM32F4 You can test in debug mode to see if the I²C is correctly configured and working or if you can directly check the electric signals.

May I also suggest you to use the syntax highlighter for your code example to ease the readability.

I hope this will help you in your debugging

.

Best Regards.