Skip to main content
Nikhil D&K
Associate III
October 31, 2022
Solved

Steps to perform Firmware Upgrade using ST25DV dynamic tag

Hello,

I would like to know how can i perform the Device Firmware upgrade using ST25DV dynamic tag.I am using "en.STSW-ST25DV001SC-Source_v1.2.0" and tried out both demonstration examples

  1. ST25DVDemo ( firmware update using internal flash)

I am able to perform firmware update using ST25DV demo example, but after reset it jumps to original firmware.

So i would like to know how can i implement a firmware upgrade feature using "ST25DVDemo" example so that after reset it boots to the uploaded firmware instead of the old firmware.

Thanks,

Nikhil.

    This topic has been closed for replies.
    Rene Lenerve
    Rene LenerveBest answer
    ST Employee
    November 7, 2022

    Hi @NK.13omalan​,

    Ok, with the dual bank I will list 3 ways to proceed, let me just summarize the concept for the dual bank.

    Double bank means the MCU has 2 flash memory areas which can be remapped using a dedicated option bytes. This remap allows to set the boot address to the bank1 or bank2 by resetting or setting this option byte. So, no need to change vector table address and compilation address with both firmware (original or updated),

    Option 1 : Original firmware is programmed in Bank1 (0x08000000), when doing firmware upgrade the new firmware is programmed at Bank2 address (0x08080000). When update is done the option byte BFB2 must be set to swap Bank address, then reset MCU to boot each time on Bank2 (now at 0x08000000) and Bank1 adress will be remapped at 0x08080000. You can repeat the operation but with Bank1 this time which will receive the new firmware (and so on).

    Option 2 : Original firmware in Bank1, Firmware upgrade firmware on Bank2. When performing the firmware upgrade swap Bank to Bank2 first to run the firmware upgrade procedure then erase Bank1, program with the new firmware and swap again to reboot to the new firmware.

    Option 3 : This is a on the fly firmware upgrade using RAM, here is the link for all the details on that technique https://www.st.com/content/ccc/resource/technical/document/application_note/group0/ab/6a/0f/b7/1a/84/40/c3/DM00230416/files/DM00230416.pdf/jcr:content/translations/en.DM00230416.pdf

    Another documentation that could give you some information on booting with STM32 : https://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

    You can find an example of code in the package stm32CubeL4 to perform the Bank swapping (https://www.st.com/en/embedded-software/stm32cubel4.html) in the folder Projects\NUCLEO-L476RG\Examples\FLASH\FLASH_DualBoot.

    I hope this gives you more details on how to proceed.

    Kind Regards.

    36 replies

    Rene Lenerve
    ST Employee
    November 7, 2022

    Hi @NK.13omalan​,

    The demo is just a demonstration on how to exchange data between reader and tag using the mailbox feature of the tag, among the possibilities is to perform a firmware update. That's why after the reset it returns to the original firmware.

    There is different ways to perform a firmware upgrade, but what to have in mind first is that you can't read and write flash memory in the same time. So, to perform a firmware upgrade you need to write the new firmware in another area of the flash memory than the current code executed, and start to this new location at boot.

    For the STM32F405 MCU you need to code a bootloader and place it at the start address then jump to the firmware address updated (this needs some configuration in your different firmwares).

    Some MCUs have a dual bank feature that allows to switch between banks at boot (unfortunately not the F405).

    Using also an external flash memory may help, but not available on the demo kit.

    Using the STM32's bootloader located in ROM, but it will require you to add an additional MCU to communicate with the bootloader code (many interfaces are available in that case UART, I²C, SPI, ...), not available on the disco kit too.

    I hope this will help you.

    Kind Regards.

    Nikhil D&K
    Associate III
    November 7, 2022

    Hello @Rene Lenerve​, thanks for reply.

    We are using STM32L496 board whose memory organization shows that it is divided in dual bank. So i will be leveraging that for the firmware upgrade implementation.

    The downloaded firmware will be written at the Bank 1 of memory, while Bank 0 will be running my application code.

    So can you please elaborate the steps of using dual bank for the firmware upgrade. From the code, i understood that i will be writing firmware to the Dual Bank 1 address.

    But after that what will be the further steps for upgrade ?

    Rene Lenerve
    Rene LenerveBest answer
    ST Employee
    November 7, 2022

    Hi @NK.13omalan​,

    Ok, with the dual bank I will list 3 ways to proceed, let me just summarize the concept for the dual bank.

    Double bank means the MCU has 2 flash memory areas which can be remapped using a dedicated option bytes. This remap allows to set the boot address to the bank1 or bank2 by resetting or setting this option byte. So, no need to change vector table address and compilation address with both firmware (original or updated),

    Option 1 : Original firmware is programmed in Bank1 (0x08000000), when doing firmware upgrade the new firmware is programmed at Bank2 address (0x08080000). When update is done the option byte BFB2 must be set to swap Bank address, then reset MCU to boot each time on Bank2 (now at 0x08000000) and Bank1 adress will be remapped at 0x08080000. You can repeat the operation but with Bank1 this time which will receive the new firmware (and so on).

    Option 2 : Original firmware in Bank1, Firmware upgrade firmware on Bank2. When performing the firmware upgrade swap Bank to Bank2 first to run the firmware upgrade procedure then erase Bank1, program with the new firmware and swap again to reboot to the new firmware.

    Option 3 : This is a on the fly firmware upgrade using RAM, here is the link for all the details on that technique https://www.st.com/content/ccc/resource/technical/document/application_note/group0/ab/6a/0f/b7/1a/84/40/c3/DM00230416/files/DM00230416.pdf/jcr:content/translations/en.DM00230416.pdf

    Another documentation that could give you some information on booting with STM32 : https://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

    You can find an example of code in the package stm32CubeL4 to perform the Bank swapping (https://www.st.com/en/embedded-software/stm32cubel4.html) in the folder Projects\NUCLEO-L476RG\Examples\FLASH\FLASH_DualBoot.

    I hope this gives you more details on how to proceed.

    Kind Regards.

    Nikhil D&K
    Associate III
    November 8, 2022

    Hello @Rene Lenerve​ , thanks for information. I will go forward with option 2 as it seems to be more standard way.

    We also have a PC software developed in C# for doing the firmware update alongside our product. We have implemented the READ ID and PRESENT_PASSWORD steps, where READ_ID is used for getting the current firmware version as response and PRESENT_PASSWORD is used for granting access to update firmware.

    Now i would like to know how to send the (.bin) file provided in the demo folder for the firmware upgrade. Because the header byte (byte containing inSegment, segId, position, ackCtrl, pktLen, type) of the payload changes with the starting segment, intermediated packets and ending segment. So how to keep track of that on the PC software side, how the calculation is done such that i know which header byte is needed to be sent, because i don't know how the starting segment and ending segment is also calculated.

    Here is the log from STM32L4 of the first packet received after of the upgraded firmware during the firmware transfer process (i.e after successful password authentication)

    [12:06:52:556] 18825 RxState = FTM_READ_IDLE�??�?�
    [12:06:52:560] 18828 RxState = FTM_READ_CMD�??�?�
    [12:06:52:658] Alert pin INT �??�?�
    [12:06:52:664] 18933 Rx-->0x15,0x0,0x0,0x6d,0x7d,0x4,0x40,0x24,0x0,0x20,0xa1,0x1,0xa,0x8,0xe3,0x3b,0xa,0x8,0x21,0x2b,0xa,0x8,0x25,0x37,0xa,0x8,0x75,0x11,0xa,0x8,0x95,0x49,0xa,0x8,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x53,0x44,0xa,0x8,0xc5,0x11,0xa,0x8,0x0,0x0,0x0,0x0,0xe5,0x3b,0xa,0x8,0x31,0x45,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xb9,0x12,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,0x8,0xbb,0x1,0xa,�??�?�
    [12:06:52:764] 19034 pkt.length - 0xf4�??�?�
    [12:06:52:769] 19036 pkt.totalLength - 0x6d7d�??�?�
    [12:06:52:769] 19039 pkt.ctrl.byte - 0x15�??�?�
    [12:06:52:774] 19042 pkt.crc - 0x0�??�?�
    [12:06:52:774] 19044 pkt.has_crc - 0x0�??�?�
    [12:06:52:780] 19046 Starting Segment 0�??�?�
    [12:06:52:780] 19048 GetCrc 2004fe5d 244�??�?�
    [12:06:52:780] TEST : 0x4�??�?�
    [12:06:52:786] 19052 ST25FTM_GetCrc : 0xd96be537�??�?�

    And below is the some packet frames decoded to get understanding. Here you can see the header bytes change for the packet. The logs below are stripped out and the packets received at the time of the new starting segment and ending segment are only displayed.

     
    Firmwware Update 
     
     
    1st frame: 
     ST25FTM_Ctrl_Byte_t : 0x15
     
     inSegment :1
     segId: 0;
     position: ST25FTM_FIRST_PACKET (01);
     ackCtrl: 01 
     pktLen: 0;
     type : 0
     
    Starting Segment 0
     
     
     
    2nd frame: 
     ST25FTM_Ctrl_Byte_t : 0x09
     
     inSegment :1
     segId: 0;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 00
     pktLen: 0;
     type : 0
     
     
    intermediate frame: 
     ST25FTM_Ctrl_Byte_t : 0x69
     
     inSegment : 1
     segId: 0;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 10
     pktLen: 1;
     type : 0
     
     
    Ending Segment 0
     
     
     
    intermediate frame: 
     ST25FTM_Ctrl_Byte_t : 0x1b
     
     inSegment : 1
     segId: 1;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 01
     pktLen: 0;
     type : 0
     
     
    Starting Segment : 1
     
     
     ST25FTM_Ctrl_Byte_t : 0xb
     
     inSegment : 1
     segId: 1;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 00
     pktLen: 0;
     type : 0
     
    .
    .
    ,
    ,
     
     ST25FTM_Ctrl_Byte_t : 0x6b
     
     inSegment : 1
     segId: 1;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 10
     pktLen: 1;
     type : 0
     
     
    Ending Segment 1
     
     
     ST25FTM_Ctrl_Byte_t : 0x19
     
     inSegment : 1
     segId: 0;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 01
     pktLen: 0;
     type : 0
     
     
    Starting Segment : 2
     
     ST25FTM_Ctrl_Byte_t : 0x09
     
     inSegment :1
     segId: 0;
     position: ST25FTM_MIDDLE_PACKET (10);
     ackCtrl: 00
     pktLen: 0;
     type : 0

    So can you please elaborate how the firmware packets (in the form of chunks) are sent from the App/PC software so that i can apply the same logic in my custom desktop application.

    Rene Lenerve
    ST Employee
    November 8, 2022

    Hi @NK.13omalan​,

    You seem to have downloaded sources for the ST25DV-DISCOVERY kit which is based on discovery board which embeds a STM32F405 MCU. May I suggest you to download sources from the ST25DV64KC-DISCO kit which embeds an STM32L476 (Link STSW-ST25DV002), this will be closer to your MCU (especially for flash management).

    In the User Manual of this disco kit the protocol used in the demo is described and the header data explained. Let me know which information is missing to build segments and packets in order to help you better?

    Kind Regards.

    Nikhil D&K
    Associate III
    November 11, 2022

    Hello @Rene Lenerve​ , thanks for information. I will be referring the docs you mentioned above.

    Currently ,I have successfully stored the received firmware packets to this address (0x080A0000) of the Bank 2 of the STM32L4 by referring the firmware package "STSW-ST25DV002" as mentioned by you. Meanwhile my application firmware is running on Bank 1.

    Now in example after successful firmware upgrade i have to touch anywhere on screen to start the upgraded firmware (i.e on touching screen the MSP is set to the upgraded firmware address and a calls to a JUMP function , which runs the upgraded firmware).

    In my case as i don't have any touch screen in my product, i have set the MSP to new firmware address(ADDRESS 0x080A0000 in BANK2 ) and calling JUMP function result into a hard fault condition.

    Here , is the code i am referring to jump.

    /**
     * @brief Jump to user program.
     * @param None No parameters.
     * @return None.
     */
    void COMMAND_Jump( void )
    {
     
     /* Jump to user application */
     JumpAddress = *(__IO uint32_t *)(FIRMWARE_ADDRESS + 4);
     Jump_To_Application = (pFunction) JumpAddress;
     /* Initialize user application's Stack Pointer */
     __set_MSP( *(__IO uint32_t *)FIRMWARE_ADDRESS );
     Jump_To_Application( );
    }

    Can you suggest what could be the issue here ?

    Rene Lenerve
    ST Employee
    November 14, 2022

    Hi @NK.13omalan​,

    Jumping to another firmware at a specific address was not your first intention according to your previous posts. To do this, you have to change the compilation parameters (mainly the scatter file) and especially the address of the vector table.

    But the option with the dual bank lets you get rid of that. the only action you need to perform in this case is to switch the bank order and reset the MCU.

    According to the examples in stm32CubeL4 package, after writing the firmware in the correct bank (take care to check that 0x080A0000 is the correct beginning address of the second Bank of your MCU, this could be different from MCUs), you should do the following operation, please read the Reference Manual of your MCU (flash section, option bytes), these options are used to customized the general settings of your MCU, but misused can lead to unwanted effects that can brick your MCU :

    HAL_FLASH_Unlock();
    	 
     /* Clear OPTVERR bit set on virgin samples */
     __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
     
     /* Allow Access to option bytes sector */ 
     HAL_FLASH_OB_Unlock();
     
     /* Get the Dual boot configuration status */
     HAL_FLASHEx_OBGetConfig(&OBInit);
     
     /* Enable/Disable dual boot feature */
     OBInit.OptionType = OPTIONBYTE_USER;
     OBInit.USERType = OB_USER_BFB2;
     
     /* Swap between Bank1 and Bank2, to adapt to use case */
     if (((OBInit.USERConfig) & (OB_BFB2_ENABLE)) == OB_BFB2_ENABLE)
     { /* Bank1 mapped to 0x00000000 at boot */
     OBInit.USERConfig = OB_BFB2_DISABLE;
     }
     else
     { /* Bank2 mapped to 0x00000000 at boot */
     OBInit.USERConfig = OB_BFB2_ENABLE;
     }
     
     if(HAL_FLASHEx_OBProgram (&OBInit) != HAL_OK)
     {
     /*
     Error occurred while setting option bytes configuration.
     User can add here some code to deal with this error.
     To know the code error, user can call function 'HAL_FLASH_GetError()'
     */
     /* Infinite loop */
     while (1)
     {
     BSP_LED_On(LED3);
     }
     }
     
     /* Start the Option Bytes programming process */ 
     if (HAL_FLASH_OB_Launch() != HAL_OK)
     {
     /*
     Error occurred while reloading option bytes configuration.
     User can add here some code to deal with this error.
     To know the code error, user can call function 'HAL_FLASH_GetError()'
     */
     /* Infinite loop */
     while (1)
     {
     BSP_LED_On(LED3);
     }
     }
     
     /* Prevent Access to option bytes sector */
     HAL_FLASH_OB_Lock();
     
     /* Disable the Flash option control register access (recommended to protect 
     the option Bytes against possible unwanted operations) */
     HAL_FLASH_Lock();

    I hope this can help you.

    Kind Regards.

    Nikhil D&K
    Associate III
    November 14, 2022

    Hello @Rene Lenerve​ , thanks for information.

    As quoted by you, 

    " But the option with the dual bank lets you get rid of that. the only action you need to perform in this case is to switch the bank order and reset the MCU. "

    By the above statement did you mean the "Option 1" which you have mentioned in the previous reply, right ? And this won't apply to "Option 2" which also use both the banks.

    Regarding OPTION 1:

    Query 1 :

    Currently the Bank 1 (Main program) is at 0x08000000 and the upgraded firmware is on Bank 2 at address 0x08080000. 

    The code snippet which you have shared (i.e Setting BFB2 byte), will be called after successfully validating the written firmware (upgraded) at the Bank 2 starting address. Now calling the reset function will swap the bank address (i.e Bank 2 -> 0x08000000 and Bank 1 -> 0x08080000) and execute the updated program from Bank 2. So do i need to keep the track of the last updated bank or address (i.e where the upgraded firmware was last downloaded) ?

    By the looks of it, it seems very simple. I have to just download the firmware at address 0x0808000 every time, than verify it. If verification (CRC) is successful, set the BFB2 option byte (i.e using the code snippet given by you above) and reset the board. It will boot with the newly upgraded firmware. Is that right ?

    Query 2 :

    I have read the Firmware upgrade process from the document "UM2949 stswst25dv002-firmware-for-the-st25dv64kcdisco-board-stmicroelectronics" as mentioned by you previously.

    In the demo firmware code, i can see the the CRC verification happening after transmission of every segment (i.e 20 packets). So if i do CRC checking for every received segment, do i have to verify the final checksum of the whole firmware received or CRC checking of the each segment is enough ? I know it will be consuming more time if i verify the firmware checksum but would like to know the standard steps. 

    Query 3:

    Currently the L4 ST25DV example flash write length is set to 512 bytes in function "FTM_FlushToFlash". Can't we increase the length to 1024 or 2048 bytes?

    We successfully tried with writing 1024 bytes but failed writing 2048 bytes in one go. 

    Regarding OPTION 2:

    If we use option 2, we have to implement custom boot loader, right ? Than we have to use magic number to know if new firmware is available.

    Rene Lenerve
    ST Employee
    November 14, 2022

    Hi @NK.13omalan​,

    Option 1 and 2 are using Dual Bank feature, using BFB2 to swap banks. The difference between Option1 and Option2 is for the former, you alternately program the firmware in each bank (which must embeds the firmware upgrade in code), for the latter you have firmware for firmware upgrade in one bank swapping only when you need to upgrade your firmware and you only program the other bank.

    Boot Loader is used without Bank swapping and needs some configuration to be implemented (another story).

    Query 1:

    That's right, and the swap to the new bank is permanent (until you overwrite this BFB2 of course).

    Query 2:

    You can use the CRC IP in Accumulate mode so you can inject data throughout firmware transfer. But you also have the option of doing it all at once at the end.

    Query 3:

    It depends on the size of your FLASH (and each Bank is half the size of the flash memory, may be your issue with 2048 bytes).

    Kind Regards.

    Nikhil D&K
    Associate III
    November 15, 2022

    Hello @Rene Lenerve​ , thanks for clarification.

    Before directly testing the dual bank swap on the downloaded upgraded firmware via NFC, i though of testing the dual bank swap with two demo application program.

    Main Program (Bank 1 :0x08000000): Blinking on-board led at interval of 2 seconds. After 10 toggles, i am calling the function toggleBankAndReset which contains code which you provided yesterday to swap banks and reset.

    Upgraded Program (Bank 2: 0x08080000): Blinking on-board led at interval of 500 milli-seconds.

    void toggleBankAndReset() {
     FLASH_OBProgramInitTypeDef OBInit;
     HAL_FLASH_Unlock();
     __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
     HAL_FLASH_OB_Unlock();
     HAL_FLASHEx_OBGetConfig(&OBInit);
     
     OBInit.OptionType = OPTIONBYTE_USER;
     OBInit.USERType = OB_USER_BFB2;
     
     if (((OBInit.USERConfig) & (OB_BFB2_ENABLE)) == OB_BFB2_ENABLE) {
     OBInit.USERConfig = OB_BFB2_DISABLE;
     } else {
     OBInit.USERConfig = OB_BFB2_ENABLE;
     }
     if (HAL_FLASHEx_OBProgram(&OBInit) != HAL_OK) {
     // uint32_t errorCode = HAL_FLASH_GetError();
     while (1) {
     HAL_Delay(1000);
     HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
     }
     }
     if (HAL_FLASH_OB_Launch() != HAL_OK) {
     //uint32_t errorCode = HAL_FLASH_GetError();
     while (1) {
     HAL_Delay(100);
     HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
     }
     }
     HAL_FLASH_OB_Lock();
     HAL_FLASH_Lock();
    }

    In Main program, on calling the function toggleBankAndReset the device hangs (breaks) and no upgraded firmware is loaded even after pressing reset.

    I have used STM32 Cube Programmer to flash the upgraded firmware at the Bank 2 address directly.

    If possible can you provide me main.c file which implements the dual bank swap for demo purpose.

    Rene Lenerve
    ST Employee
    November 15, 2022

    Hi @NK.13omalan​,

    Reading the Reference manual of the STM32L496 there is a note saying that when swapping to Bank 2 you need to relocate the vector table.

    "Note: When booting from bank 2, the boot loader will swap the Flash memory banks.

    Consequently, in the application initialization code, you have to relocate the vector table to

    bank 2 swapped base address (0x0800 0000) using the NVIC exception table and offset

    register."

    So it it is probably the reason why it doesn't boot. Sorry for the confusion on this point.

    Hope this can help you.

    Kind Regards.

    Nikhil D&K
    Associate III
    November 15, 2022

    Hello @Rene Lenerve​ ,

    Does that mean i have to call NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x4000) function. And if yes, were should i call this function before HAL_Init() in upgraded firmware ?

    Rene Lenerve
    ST Employee
    November 15, 2022

    Hi @NK.13omalan​,

    You probably can use it before calling HAL_Init() (I didn't try it so I'm not sure if it works correctly). but the new vector table is at the first address of the firmware, so where you programmed your binary.

    So maybe you probably need to change the value of VECT_TAB_OFFSET in system_stm32l4xx.c to match the correct address too, and the scatter file to set firmware address to the linker.

    Kind Regards.

    Nikhil D&K
    Associate III
    November 16, 2022

    Hello @Rene Lenerve​,

    We were able to perform a sample firmware update using the ST25DV_Demo example running on STM32L496 as our main firmware (Bank 1) and the demo upgraded firmware we selected was FLASH_DualBoot_Bank2 project present in the official repository.

    Path for the upgraded firmware (FLASH_DualBoot_Bank2) :

    " STM32Cube_FW_L4_V1.17.2/Projects/NUCLEO-L496ZG/Examples/FLASH/FLASH_DualBoot/SW4STM32/FLASH_DualBoot_Bank2 "

    We are able to switch banks from the ST25DV_DEMO Bank1 firmware example to FLASH_DualBoot_Bank2 example running on Bank 2. When the device is running the FLASH_DualBoot_Bank2 , on user button press we were able to swap the banks again and were able to run NFC example again.

    You can check out the main.c code in FLASH_DualBoot_Bank2 for reference.

    Query 1:

    Now the issue arises when i want to use different example for upgrading purpose instead of the FLASH_DualBoot_Bank2 example. For say if i am running ST25DV_Demo example on Bank1 . And i want to upgrade to firmware similar to ST25DV_Demo example with newer major minor version info and led blinking added to it to differentiate between examples in Bank 1 and Bank 2. I am successfully able to write to Bank 2 the modified ST25DV_Demo example but after swapping the bank the firmware doesn't work after swap.

    Note: We also tried using simple blinky example for Bank 2, but that also didn't worked. We were only able to successfully upgrade using DuablBootBank2 example.

    What could be the reason here because i am able to successfully upgrade to FLASH_DualBoot_Bank2 example but unable to upgrade to modified ST25DV_Demo example ?

    Query 2:

    I also wanted to know how the controller get reseted after we set the BFB2 byte, because i don't see anywhere reset function being called.

    Rene Lenerve
    ST Employee
    November 18, 2022

    Hi @NK.13omalan​,

    There is some threads in the MCU section of the ST community forum that mention issues with the reboot on some boards (for dual bank) and they have to use this function to reset : HAL_NVIC_SystemReset(); after HAL_FLASH_OB_Launch();.

    Your question has shifted from the tag issue to an MCU issue, you should post this kind of question in the MCU section to have more people aware about this topic (This thread is mostly read by people aware about NFC tags and readers).

    Kind Regards.

    Nikhil D&K
    Associate III
    December 2, 2022

    Hello @Rene Lenerve​ ,

    Thanks for support we were able to successfully perform the firmware update.

    I would like to know, is there any easy way of migrating code made for ST25DV04K to ST25DV04KC.

    And do i have to make any changes in my Desktop application for communicating with ST25DV04KC ? Currently desktop application is successfully able to communicate with ST25DV04K using ST25R3911B software.

    And is ST25DV04K obsolete ?

    Rene Lenerve
    ST Employee
    December 2, 2022

    Hi @NK.13omalan​,

    There are some minor changes between ST25DV04K and ST25DV04KC and it mainly impacts firmware. You can have a look in the AN5633: Migrating from ST25DVxxK to ST25DVxxKC (https://www.st.com/content/ccc/resource/technical/document/application_note/group1/0f/6b/06/3d/eb/bd/48/03/DM00776361/files/DM00776361.pdf/jcr:content/translations/en.DM00776361.pdf) to get more information.

    So, you shouldn't have to change anything on your Desktop Application (or maybe only if you read some registers the content might be a little bit different, you can check AN5633 in that case).

    On firmware side, you need to get component drivers for the ST25DVxxKC, as there is some changes on some registers and BSP drivers too. But, normally if you already get the STSW-ST25DV002 package, you have both drivers used in the demo, and you can have an example on how to manage both components in the same code.

    I hope this can help you on your development.

    Kind Regards.

    Nikhil D&K
    Associate III
    December 2, 2022

    Hello, i would also like to know is ST25DV04K is obsolete ?