Skip to main content
EAw.1
Associate
May 27, 2021
Solved

ST25SDK-1.8.0 ST25PcDemoApp Error "%1 is not a valid Win32 application"

I follow the ST25PcDemoApp_software_guide in ST25SDK-1.8.0 but I encountered an error at streader.dll.

"java.lang.UnsatisfiedLinkError: C:\Users\DengKai\workspace\st25PcDemoApp\resources\windows\x86\streader.dll: %1 is not a valid Win32 application"

How do I solve this error?

    This topic has been closed for replies.
    Damien G.Best answer
    ST Employee
    June 2, 2021

    Hello Eumund,

    another possible cause for the error could be the use of a 64-bit jdk instead of a 32-bit version.

    Make sure your folder to the jdk points to the C:\Program Files (x86)\Java\jdk directory instead of C:\Program Files\Java\jdk

    3 replies

    ST Employee
    May 27, 2021

    Hello,

    the UnsatisfiedLinkError is typical of your environment path not containing the location of the streader dll file.

    I invite you to check the answer to this question.

    Basically, you have to ensure that your path contains the location of \resources\windows\x86\

    Best regards,

    Damien

    EAw.1
    EAw.1Author
    Associate
    May 28, 2021

    Hi Damien,

    I referred to the link you gave to me, I had ensured that all the path(Source Path & Environment Path) contains the correct location of \resources\windows\x86\. However, the problem still persists.

    Best Regards,

    Eumund

    Damien G.Best answer
    ST Employee
    June 2, 2021

    Hello Eumund,

    another possible cause for the error could be the use of a 64-bit jdk instead of a 32-bit version.

    Make sure your folder to the jdk points to the C:\Program Files (x86)\Java\jdk directory instead of C:\Program Files\Java\jdk