Skip to main content
Prabhu1
Associate II
May 11, 2021
Solved

ST25RU3993 : Is the power output is calibrated? What would be the tolerance.?

When I set the tx power as 25 dBm in the application what would be output tolerance.

What would be the output power accuracy?

We understand that tolerance resolution would be the parameter to drive the step size.

Regards

Prabhu

This topic has been closed for replies.
Bart Herse
Bart HerseBest answer
Visitor II
May 27, 2021

Dear Skann.1,

For both readers ST25RU3993-EVAL and ST25RU3993-HPEV the output power level is not calibrated.

A closed-loop output power control can be implemented using the power detector that is present on the boards.

The output power level resulting to 25 dBm is for both readers at Ant1:

  • ETSI: -7
  • FCC: -6

For the tolerances you can expect approx. +/- 1.2 dB

I hope this information is helpful.

Cheers,

B

1 reply

Bart Herse
Bart HerseBest answer
Visitor II
May 27, 2021

Dear Skann.1,

For both readers ST25RU3993-EVAL and ST25RU3993-HPEV the output power level is not calibrated.

A closed-loop output power control can be implemented using the power detector that is present on the boards.

The output power level resulting to 25 dBm is for both readers at Ant1:

  • ETSI: -7
  • FCC: -6

For the tolerances you can expect approx. +/- 1.2 dB

I hope this information is helpful.

Cheers,

B