Skip to main content
NBert.1
Visitor II
September 6, 2021
Solved

ST25RU3993-HPEV pre-tuning algorithm

Hi, I am working with the ST25RU3993 HPEV board. 

I have configured the API with the USA frequency profile and every time I launch a new inventory it runs the pre-tuning algorithm which takes about 17 seconds. 

Is there any way to avoid this? I mean, some functionality that stores the tuning parameters and applies them every time an inventory is executed?

BR, Nicolas

  

This topic has been closed for replies.
Bart Herse
Bart HerseBest answer
Visitor II
September 14, 2021

Hello NBert.1,

it is possible to disable the pre tuning in the reader settings under the Tuning tab.

Alternatively the pre tuning algorithm can be changed to FAST or VERYFAST. This way the pre tuning is still done but the convergence time is shorter.

Note that once a tuning file is generated for specific frequency range and, most important, downloaded to the reader, the tuning will be stored permanently to the reader.

So next time the reader is powered up the previously stored tuning will be applied.

Cheers,

B

1 reply

Bart Herse
Bart HerseBest answer
Visitor II
September 14, 2021

Hello NBert.1,

it is possible to disable the pre tuning in the reader settings under the Tuning tab.

Alternatively the pre tuning algorithm can be changed to FAST or VERYFAST. This way the pre tuning is still done but the convergence time is shorter.

Note that once a tuning file is generated for specific frequency range and, most important, downloaded to the reader, the tuning will be stored permanently to the reader.

So next time the reader is powered up the previously stored tuning will be applied.

Cheers,

B