Skip to main content
MPrzy.1
Associate
August 11, 2020
Solved

ST25RU3993 eval low output level

Hello,

I've observed that output level on both antenna port is lower than is specified in datasheet. I've checked it on two eval boards. Below results:

For internal PA: (output level set/ measured level/ detector voltage

  1. -12 / 4,5 dBm / 0 ,71V
  2. -6 / 8,9 dBm / 0,81V
  3. 0 / 12,2 dBm /0,89V

For external PA:

  1. -12 / 14,4 dBm , / 0,92V
  2. -6 / 19,5 dBm / 1,05V
  3. - 3 / 20,8 dBm / 1,08V
  4. 0 / 21,5 dBm / 1,1V

In both cases output level is lower by 7-8 dBm that expected. Any suggestion?

Best Regards, Michał

This topic has been closed for replies.
MPrzy.1
MPrzy.1Best answer
Associate
August 12, 2020

Problem probably solved and was in my spectrum analyzer malfunction.

Michal

1 reply

MPrzy.1
MPrzy.1AuthorBest answer
Associate
August 12, 2020

Problem probably solved and was in my spectrum analyzer malfunction.

Michal