Skip to main content
KFin.1
Associate
March 3, 2020
Solved

ST25RU3993-EVAL: I can't switch to internal PA => TX setting failed

I'm running a ST25RU3993-EVAL with firmware version V2.0.0.0 STUHFL. Under "Reader Settings" in tab "Settings" under "EU Profile", within the TX-Options, there is a Selection-Field "Internal/External PA", which by default is set to external PA.

When I try to set this to internal PA, I do get an error message "TX setting failed".

Has anyone an idea, if this feature is possibly disabled by firmware, or even not yet implemented?

    This topic has been closed for replies.
    Marcel Rossignol
    Marcel RossignolBest answer
    ST Employee
    March 5, 2020

    Hi,

    thank you for this hint!

    We could reproduce this issue and in the next GUI Version 2.0.2.0 it will be possible to switch between the Internal/External PA.

    Best regards,

    Marcel

    2 replies

    Marcel Rossignol
    Marcel RossignolBest answer
    ST Employee
    March 5, 2020

    Hi,

    thank you for this hint!

    We could reproduce this issue and in the next GUI Version 2.0.2.0 it will be possible to switch between the Internal/External PA.

    Best regards,

    Marcel

    KFin.1
    KFin.1Author
    Associate
    March 5, 2020

    Hi,

    and thanks a lot for the response!

    I'm looking forward to testing the next GUI release ...

    Best regards,

    KFIN