Skip to main content
David3
Visitor II
August 28, 2018
Question

ST25RU3993-EVAL Board + Tags

Unable to get ST25RU3993-EVAL Board as it does not appear to be available, have all the details of board if we construct this Evaluation board would we be able to load the firmware into it and use the PC software and it work ok?

Second question, there are no ST UHF Tags available could not find any on ST site all the ones at any distributors (all obsolete) we have found some made by NXP I assume these will work with the ST25RU3993?

    This topic has been closed for replies.

    2 replies

    Bart Herse
    Visitor II
    September 12, 2018

    Hello,

    boards are available please contact your local ST contact.

    If you build the board exactly as is then the code will load and the board should work.

    ST currently offers no Rain (UHF) tags.

    The reader IC works with tags from other vendors.

    Cheers,

    B.

    Raphael K
    Associate
    October 12, 2018

    Good day,

    based on the ST25RU3993 and an STM32, we have built our own board with 8 antenna outputs. Is it possible to get the source code of the PC software (STSW-ST25RU001) so that we can extend it to 8 antennas?