Skip to main content
Franco Bocalon
Associate II
September 25, 2019
Solved

ST25RU3993-EVAL board. Autotuning feature

  • September 25, 2019
  • 4 replies
  • 1024 views

The autotuning algorithm implemented in the app reader, is an external routine? I mean, the IC ST25RU3993 by itself can not tune an antenna. I guess that we need to implement some algorithm making a sweep and checking the reflected power, and then finally set the 3 values for the tunning capacitors.

This topic has been closed for replies.
Best answer by Nick K

​Hi, the tuning algorithms are all completly implemented in the FW, the "Reader Suite" application simple call them in the FW. You find all the necessary implementation in the file "tuner.c". The 4 algorithms are implemented in the following functions "tunerOneHillClimb" -> FAST, "tunerDuplicatedOneHillClimb" -> VERYFAST, "tunerMultiHillClimb" -> SLOW and "tunerEnhancedMultiHillClimb" -> MEDIUM.

Hope this answers  your question, if you have further questions let me know.

BR Nick

4 replies

Nick K
ST Employee
September 26, 2019

Hello, yes correct. The carrier cancelation circuite​ is a external HW component that is controlled by an MCU (The same MCU that controlls also the ST25RU3993). As an example how this could look like in HW and how it is used in FW please have a look into the EVAL board schematic and the EVAL board FW. Both could be found on www.st.com

Best Regards

Franco Bocalon
Associate II
September 26, 2019

Dear Nick, Hi. I understand. But I mean that the search algorithms (OneHillClimb, MultiHillClimb, DuplicatedFastHillClimb, and EnhancedMultiHillClimb) I guess that the Appreader app implements them. I could not see this algorithms into the fw side.

Regards

Nick K
Nick KBest answer
ST Employee
September 26, 2019

​Hi, the tuning algorithms are all completly implemented in the FW, the "Reader Suite" application simple call them in the FW. You find all the necessary implementation in the file "tuner.c". The 4 algorithms are implemented in the following functions "tunerOneHillClimb" -> FAST, "tunerDuplicatedOneHillClimb" -> VERYFAST, "tunerMultiHillClimb" -> SLOW and "tunerEnhancedMultiHillClimb" -> MEDIUM.

Hope this answers  your question, if you have further questions let me know.

BR Nick

Franco Bocalon
Associate II
September 26, 2019

Dear Nick,

I am sorry. I could find them before.

Thank you so much.

Best Regards

Franco