Associate III
March 4, 2024
Solved
ST25R95 Jumps out of IDLE without tag - Custom Hardware
- 3 replies
- 1503 views
I am working off of Custom Hardware using the ST25R95 and I can read tags but I am trying to keep the device into IDLE mode but can't get it to work.
I have ran tag detect calibration without a tag in the field and came up with a result of 0x5C. (See attached Traces from boot)
I used 0x5C as the base for IDLE mode and use the +/-0x08 to setup the thresholds.
Using 0x5C, the device keeps telling me that there is a tag and starts to read a tag, goes into IDLE and repeats without a tag in the field. (See attached Traces from boot).
Do you have any ideas why this will not stay in IDLE?