Skip to main content
suads
Associate III
Aug 4, 2020 1:11 PM UTC
Solved

ST25R95 IRQ_In low pulse?

Hello ,

According to the st25r95 datasheet:

"After the power supply is established at power-on, the ST25R95 waits for a low pulse on the pin IRQ_IN (t1) before automatically selecting the external interface (SPI) and entering Ready state after a delay".

I have a custom board and I want to read the device id over spi, but the IRQ_IN pin is not connected.

Can it work without IRQ_IN low pulse? Can I communicate with the device, currently I have nothing on MISO line.

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Aug 4, 2020 4:48 PM UTC

    Hi,

    IRQ_IN needs to be connected and needs to follow the power up sequence. SPI communications can only be performed once the power up sequence is completed.

    IRQ_OUT is recommended to be connected as well.

    X-CUBE-NFC3 firmware uses both IRQ_IN and IRQ_OUT.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    1 reply

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Aug 4, 2020 4:48 PM UTC

    Hi,

    IRQ_IN needs to be connected and needs to follow the power up sequence. SPI communications can only be performed once the power up sequence is completed.

    IRQ_OUT is recommended to be connected as well.

    X-CUBE-NFC3 firmware uses both IRQ_IN and IRQ_OUT.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.