Hi,
"Transmit unmodulated" is simply a constant carrier. This can be achieved by a ProtocolSelect command with any of the reader technologies (protocol code 01: ISO/IEC 15693, 02: ISO/IEC 14443-A, 03: ISO/IEC 14443-B or 04: FeliCa).
"Transmit modulated" is simply sending some data. This can be achieved by using a SendRecv command after a reader protocol has been selected.
"Always in receive mode" applies to two way radio transceivers like walkie-talkie (i.e. when not talking, the transceiver is in receive mode and the second device can transmit its carrier). This does not apply to NFC as the tag modulates its reply on the carrier transmitted by the NFC reader (i.e. the NFC Reader sends a carrier on which the tag reply will be received). Just ignore this test or put the reader in ready mode (i.e. protocolSelect(00: FieldOff))
Rgds
BT
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.