Skip to main content
Associate
Oct 23, 2026 11:13 AM UTC
Question

ST25R500 Standalone Eval Board

Hi Team,

I am currently working on integrating the ST25R500 NFC reader using its standalone evaluation board with an external NXP MCU.

Could someone please guide me on how to connect the ST25R500 evaluation board to the NXP MCU, including the required hardware connections and interface signals?

Your support and guidance would be greatly appreciated.

Thanks in advance!

5 replies

Andrew Neil
Super User
Oct 23, 2026 11:20 AM UTC

Section 4.1 “System diagram” in the datasheet shows you how to connect any MCU - it’s just SPI plus an IRQ line.

See also Application Notes, etc, on the ‘Documentation’ tab of the Product Page:

https://www.st.com/en/nfc/st25r500.html#documentation

 

See also the ‘Tools & Software’ tab for example code:

https://www.st.com/en/nfc/st25r500.html#tools-software

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Travis Palmer
ST Employee
Oct 23, 2026 11:56 AM UTC

Hi Raky21,

 

I agree with Neil, no matter which MCU, it is just SPI + IRQ + MCU Supply (VDD_IO) for the level shifter. Lets assume the MCU (and its peripheral) is running at 3.3V and the ST25R at 5.0V, VDD_IO should be connected to the same 3.3V supply as the MCU. 

Please also have a look at the deliverables of the ST25R300 (X-NUCLEO-NFC12A1, STEVAL-25R300KA). The ST25R300 is the consumer version of the ST25R500.

BR Travis

raky21Author
Associate
Oct 24, 2026 4:04 AM UTC

​@Andrew Neil and ​@Travis Palmer ,

Thank you for the information.

The board I have is a standalone ST25R500 evaluation board connected to the N64 Interface PCB V2.
I need clarification on how to connect the following signals to my external MCU:
BSS, SCLK, MOSI, MISO, IRQ, VDD_IO, VDD, VDD_TX

I'm having difficulty understanding the pin connections and the required power supply connections for these signals.
I also tried to attach an image of the board for reference, but I couldn't upload it.

Could you please guide me on the correct connections between the ST25R500 evaluation board and my external MCU?

Additionally, I've implemented DMA-based SPI synchronous transmission on the MCU side.
In this case, how should I connect and handle the IRQ pin? Is it still required, and how should it be configured in the firmware?

Your guidance would be greatly appreciated, as I need to proceed with the integration.
Thank you for your support.

 

Raky

 

Andrew Neil
Super User
Oct 24, 2026 11:04 AM UTC

tried to attach an image of the board for reference, but I couldn't upload it.

Indeed, uploads are currently disabled:

Which, unfortunately, means I also can’t upload anything to help.

 

But it is a very basic connection: again, just standard SPI - so that will be exactly the same as connecting any other SPI slave to any microcontroller.

Did you look at the diagram in the ST25R500 datasheet?

The NXP documentation will tell you about your MCUs SPI connections & operations.

 

If you’ve never used the SPI on that MCU before, look for SPI examples provided by NXP - use them to gain familiarity.

Edited to add: I don’t know NXP processors, but DMA is usually an extra level of complication - so generally best to get things working first without it.

 

how should I connect and handle the IRQ pin? Is it still required, and how should it be configured in the firmware?

Study the ST25R500 documentation to see what it uses the IRQ pin for; think how that is appropriate to your particular application; if useful, configure appropriately.

 

Have you looked at the ST-provided code?

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Oct 24, 2026 12:07 PM UTC

ST25R500 evaluation board

Which one, exactly?

There’s no eval boards on the ST25R500 Product Page, and I couldn’t see “ST25R500 evaluation board” on the ST25 NFC/RFID eval boards page ?

Please give a link.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.