Skip to main content
Associate
September 19, 2025
Solved

ST25R39R11B

Jluu_0-1758264667716.png

Jluu_1-1758264693204.pngJluu_2-1758264767856.pngJluu_3-1758264780780.png

 

Currently, we are developing a card reader featuring a circular NFC antenna. However, due to the lack of equipment for measuring antenna parameters, we are reliant solely on calculated theoretical values. The circuit board and antenna are depicted in Figure 1, impedance matching is shown in Figure 2, and simulation diagrams are presented in Figures 3 and 4. Is there any means to optimise the antenna design or draw the antenna? Alternatively, are any circular antennas readily available? The circular antenna requires a minimum diameter of 42mm and a maximum diameter of 50mm.

 

*This post has been translated from Chinese to comply with the ST Community guidelines.

This topic has been closed for replies.
Travis Palmer
Travis PalmerBest answer
ST Employee
October 28, 2025

Hello J-luu,

 

It is not very easily possible to tune a NFC reader without VNA.

There is a nanoVNA H4, which is quite affordable. 

Even if you use a pre-tuned 50Ohm antenna, it is recommended to check the tuning. Parasitics introduced with the layout or PCB layerstack can have very bad influence on the matching. 

One other solution is to rent a service at a university or consult an external RF design house.

BR Travis

1 reply

Travis Palmer
Travis PalmerBest answer
ST Employee
October 28, 2025

Hello J-luu,

 

It is not very easily possible to tune a NFC reader without VNA.

There is a nanoVNA H4, which is quite affordable. 

Even if you use a pre-tuned 50Ohm antenna, it is recommended to check the tuning. Parasitics introduced with the layout or PCB layerstack can have very bad influence on the matching. 

One other solution is to rent a service at a university or consult an external RF design house.

BR Travis