Skip to main content
pagano.paganino
Associate III
January 17, 2020
Solved

ST25R3916 solution for exclusive use in Card Emulation mode.

Hello,

I am evaluating the ST25R3916 solution for exclusive use in Card Emulation mode.

I need additional information on the part of passive components and matching circuits necessary to use only the Card Emulation mode.

As a reference I was seeing the X-NUCLEO-NFC06A1 board, do I need all the components on the X-NUCLEO-NFC06A1?

Any reference on this?

Best regards,

Damiano

    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    January 20, 2020

    Hi Damiano,

    I had a chat with Carlo:

    With the ST25 tags it is not possible to implement an arbitrary ISO7816-4 (non-NDEF) application. Even if you don't want to use reader functionality on the ST25R3916 you still need all the components. The only exception is the Variable Capacitors which you can remove / compensate with the MLCs.

    Regards, Ulysses

    5 replies

    Carlo Corlattoni
    ST Employee
    January 17, 2020

    Hello,

    Also for card mode only it is required to use all passive components like in reader mode, including complete matching network.

    If you only need card mode, maybe you can use ST25 dynamic tags instead?

    Bye,

    Carlo

    pagano.paganino
    Associate III
    January 17, 2020

    Hello Carlo,

    i need ST25R3916 for card emulation, there are others ST25 that offer this functionality?

    Regards,

    Damiano

    Carlo Corlattoni
    ST Employee
    January 17, 2020
    pagano.paganino
    Associate III
    January 17, 2020

    I have the problem wrote in this post: https://community.st.com/s/question/0D50X0000BsOJvASQW/application-non-ndef

    There are ST25 dynamic tags that offer this functionality?

    Thanks,

    Damiano

    Ulysses HERNIOSUS
    ST Technical Moderator
    January 20, 2020

    Hi Damiano,

    I had a chat with Carlo:

    With the ST25 tags it is not possible to implement an arbitrary ISO7816-4 (non-NDEF) application. Even if you don't want to use reader functionality on the ST25R3916 you still need all the components. The only exception is the Variable Capacitors which you can remove / compensate with the MLCs.

    Regards, Ulysses