Skip to main content
OSilv.1
Associate III
October 20, 2022
Solved

ST25R3916 FIFO read strange issue (Nucleo-L433RC-P & X-Nucleo-NFC06A1)

After I write to the FIFO, I read the FIFO to check if the bytes were property transferred (I understand that I cannot read and then transmit, this is just for debugging). I have a strange issue where the number of bytes in the FIFO are exactly half of what I write. Also, the bytes themselves are not what I wrote. Each time I read from the FIFO, the number of bytes in the FIFO are halved until there are zero bytes.

Here I write to the FIFO:

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_RESET);

ret = HAL_SPI_Transmit(&hspi2, &FIFO_w, 1, 50);

ret = HAL_SPI_Transmit(&hspi2, &sof, 1, 50);

ret = HAL_SPI_Transmit(&hspi2, ppm_message, ppm_message_len, 50);

ret = HAL_SPI_Transmit(&hspi2, &eof, 1, 50);

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_SET);

And here I read the FIFO length and FIFO itself:

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_RESET);

ret = HAL_SPI_Transmit(&hspi2, &FIFO_status_addr_r, 1, 50);

ret = HAL_SPI_Receive(&hspi2, &raw_rx_len, 1, 50);

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_SET);

uint8_t raw_rx[raw_rx_len];

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_RESET);

ret = HAL_SPI_Transmit(&hspi2, &FIFO_r, 1, 50);

ret = HAL_SPI_Receive(&hspi2, raw_rx, raw_rx_len, 50);

HAL_GPIO_WritePin(SPI_SS_GPIO_Port, SPI_SS_Pin, GPIO_PIN_SET);

ppm_message[24] is: {0x20, 0x02, 0x02, 0x02, 0x08, 0x80...}

raw_rx[12] is: {0x10, 0x90, 0x01, 0x01, 0x01, 0x04, 0x40...}

the next FIFO read produces:

raw_rx[6] is: {0x01, 0x01, 0x01, 0x01, 0x04, 0x40}

and then:

raw_rx[3] is: {0x40, 0x40, 0x40}

and so on...

Its strange that the raw_rx looks vaguely like the ppm_message in terms of the pattern of repeated numbers.

Any help or guesses would be greatly appreciated!

Thanks,

Oliver

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
October 20, 2022

Hi Oliver,

shifted bit patterns indicate a wrong SPI mode being used. Please check that.

Best Regards, Ulysses

2 replies

Ulysses HERNIOSUS
ST Technical Moderator
October 20, 2022

Hi Oliver,

shifted bit patterns indicate a wrong SPI mode being used. Please check that.

Best Regards, Ulysses

OSilv.1
OSilv.1Author
Associate III
October 20, 2022

This was it. Working now with CPOL = Low and CPHA = 2 Edge.

Thank you!