Skip to main content
Hzhao.2186
Associate II
Nov 25, 2019 7:44 AM UTC
Solved

ST25R3911B with antenna size 30x30cm

Hi,

I am trying to design NFC antenna with ST25R3911B,the antenna size is about 30*30cm,and the read range need 35cm;

I want to know the target matching impedance ,and is it possible to fulfill this requirement with the ST25R3911B NFC reader?

This topic has been closed for replies.
Travis Palmer
Travis PalmerBest answer
ST Employee
Nov 29, 2019 6:50 AM UTC

​Hello Sky,

Following this two threads, you should succeed.

https://community.st.com/s/question/0D50X0000AvgiHoSQI/st25r3911b-with-antenna-size-30x40cm

https://community.st.com/s/question/0D50X00009XkWCSSA3/design-questions-around-st25r3911b

In the second thread we achieved a read range of 24cm using a 14x10 cm antenna. For you purpose I would recommend a 25x25cm or 30x30 cm antenna.

The Register 0x27 should be kept at 0x00. I would start with a target matching impedance around 15 to 20. The Q-factor should be around 35. The capacitive voltage divider should be setup in a way you achieve 2.7Vpp on the RFI (using the Measure Amplitude command).

Further information can be found in the application note "AN4974 Antenna matching for ST25R3911B/ST25R391x devices".

BR Travis

1 reply

Travis Palmer
Travis PalmerBest answer
ST Employee
Nov 29, 2019 6:50 AM UTC

​Hello Sky,

Following this two threads, you should succeed.

https://community.st.com/s/question/0D50X0000AvgiHoSQI/st25r3911b-with-antenna-size-30x40cm

https://community.st.com/s/question/0D50X00009XkWCSSA3/design-questions-around-st25r3911b

In the second thread we achieved a read range of 24cm using a 14x10 cm antenna. For you purpose I would recommend a 25x25cm or 30x30 cm antenna.

The Register 0x27 should be kept at 0x00. I would start with a target matching impedance around 15 to 20. The Q-factor should be around 35. The capacitive voltage divider should be setup in a way you achieve 2.7Vpp on the RFI (using the Measure Amplitude command).

Further information can be found in the application note "AN4974 Antenna matching for ST25R3911B/ST25R391x devices".

BR Travis