Skip to main content
Guilherme dePaula
Associate II
May 2, 2018
Solved

st25r3911b sequence to see tag

Posted on May 02, 2018 at 19:09

Hi all,

I use a dsPIC33 MCU, but I am very familiar with the STM32 as well, so I used the ST25R Dicovery source code as an example.  

The design is a PIC MCU and the ST25R3911B, (with our antenna circuitry following ST design suggestions).  I have the SPI port communication working well, and I can read/write to the ST25R registers from the MCU.

1. I currently call the initialization at power up (rfalAnalogConfigInitialize() and rfalInitialize()), with gets completed without errors.

2. I now need to know what is the sequence of commands needed to talk to a tag.  We can talk to the tag (read/write) from the

ST25R Dicovery 

PC GUI without problems, but I am not sure which commands need to be sent to achieve that in the embedded code, because I don't know the exact sequence of commands needed.  Here's what I do when I want to discover a tag placed on the antenna:

a. I call iso15693Initialize() ... no error. (trying to imitate the 'Configuration' button click on the PC GUI)

b. I call rfalFieldOnAndStartGT() ... no error.  Do I need this????

c. And trying to imitate the 'Inventory' button click on the PC GUI, I call iso15693Inventory() ... but the code gets stuck in rfalTransceiveRunBlockingTx() in this statement: while( ((ret = rfalGetTransceiveStatus() ) == ERR_BUSY) && rfalIsTransceiveInTx() ); ... it's forever waiting at RFAL_TXRX_STATE_TX_WAIT_GT state.

Also, I have rfalWorker() in my main loop in main.c

Am I missing a command in my sequence?

Or maybe, does it mean it needs the tag closer?  Is the antenna not turned on? Is it potentially a hardware problem with our antenna circuitry?

After that is achieved, I realize I still have to try to imitate 'Get System Information', 'iso15693ReadBlock' for reading blocks, 'iso15693WriteBlock', etc, etc

But am I missing anything so far just to initialize the device and then get an 'Inventory'? (before calling iso15693Inventory())

Thanks,

Gil

#iso15693 #st25r3911b-disco #st25r3911b #inventory16slot
    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    May 4, 2018
    Posted on May 04, 2018 at 14:47

    Hi Gil,

    iso15693 layer is a convenience layer (and glue layer for the GUI) using the RFAL. So you don't need both layers. For usage of the rfal layer only you could have a look at the XNUCLEO-NFC05A software (

    http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/x-cube-nfc5.html

     )

    Having it forever hanging in that loop hints on a problem on Interrupt service routine. Is it the right pin, is it high or low?

    Regards, Ulysses

    4 replies

    Ulysses HERNIOSUS
    ST Technical Moderator
    May 4, 2018
    Posted on May 04, 2018 at 14:47

    Hi Gil,

    iso15693 layer is a convenience layer (and glue layer for the GUI) using the RFAL. So you don't need both layers. For usage of the rfal layer only you could have a look at the XNUCLEO-NFC05A software (

    http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/x-cube-nfc5.html

     )

    Having it forever hanging in that loop hints on a problem on Interrupt service routine. Is it the right pin, is it high or low?

    Regards, Ulysses

    Guilherme dePaula
    Associate II
    May 4, 2018
    Posted on May 04, 2018 at 17:30

    Hi Ulysses,

    Great feedback!

    1. I will try to use just one layer (RFAL) and check out the suggested software, instead of the one I used as example.

    2. I will double-check the interrupt line pin and level/edge configurations, and if the ISR is called, etc.

    Thanks!

    Cheers,

    Gil