Skip to main content
willem buitendyk
Associate II
May 6, 2021
Solved

ST25R3911B or the ST25R3916?

I'm trying to decide between the ST25R3911B or the ST25R3916? I realize the ST25R3916 is newer; but newer does not always equal better. Are there any advantages to developing with the ST25R3911B? Primary purpose is to read 15683 transponders in a sometimes wet environment. Looking for a read range of 10cm

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
May 7, 2021

Hi willem buitendyk,

ST25R3916 is really an evolution and an almost complete super set of the ST25R3911B. The main differences of the ST25R3916 are:

  • Improved receiver (correlating including summation mode)
  • Active Wave shaping feature to meet latest standard compliance requirements
  • Card - Emulation and Passive Target support
  • AAT using Vari caps instead of capacitor banks
  • EMD handling in HW (required for standard compliance)

Please see also the slide 4 of ST25R3916_product_presentation-v1.0-Feb2019.pdf which details some more differences.

Regards, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
May 7, 2021

Hi willem buitendyk,

ST25R3916 is really an evolution and an almost complete super set of the ST25R3911B. The main differences of the ST25R3916 are:

  • Improved receiver (correlating including summation mode)
  • Active Wave shaping feature to meet latest standard compliance requirements
  • Card - Emulation and Passive Target support
  • AAT using Vari caps instead of capacitor banks
  • EMD handling in HW (required for standard compliance)

Please see also the slide 4 of ST25R3916_product_presentation-v1.0-Feb2019.pdf which details some more differences.

Regards, Ulysses