Skip to main content
EGiff
Associate II
December 4, 2018
Solved

ST25R3911B-DISCO - I2C - SCL/SDA labels on PCB are switched

I have two ST25R3911B-DISCO boards and while recently trying to communicate over I2C - after alot of troubleshooting I discovered that the labels on P203 for SCL and SDA are incorrect and have been switched.

The schematic is correct - I traced the pins through to P203 - it appears only the silkscreen is incorrect.

On the back of the card, I have MB1325 C-01 217410690

The Q/A sticker shows a line on T1, T2, T3, T4 but interestingly, not "QA"

Let me know if I can provide additional information about these boards.

This topic has been closed for replies.
Travis Palmer
Travis PalmerBest answer
ST Employee
December 13, 2018

​Dear Evan,

Yes the label SCL and SDA of P203 are swapped.

We will fix this in the next HW / SW release.

Many Thanks,

BR Travis

2 replies

EGiff
EGiffAuthor
Associate II
December 12, 2018

Also, in the firmware provided by ST - the I2C initialization code is also incorrect.

In the file STSW-ST25R002 - "Sources of STM32L4 based firmware for ST25R3911B-DISCO" -

In the method HAL_I2C_MspInit in stm32l4xx_hal_msp.c we find:

...

   GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_8;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;

   GPIO_InitStruct.Pull = GPIO_PULLUP;

   GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

   GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;

   HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

This is incorrect - the I2C pins for I2C 1 are PB8 and PB9, not PB7 and PB8.

The result is that, even with the pins corrected - I2C will still not work without this correction in the firmware as well.

   GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;

Travis Palmer
Travis PalmerBest answer
ST Employee
December 13, 2018

​Dear Evan,

Yes the label SCL and SDA of P203 are swapped.

We will fix this in the next HW / SW release.

Many Thanks,

BR Travis