Skip to main content
NPeze.2138
Visitor II
Dec 8, 2019 12:51 AM UTC
Solved

ST25R3911B-DISCO compliant tags

I would like to find out if the eval board ST25R3911B-DISCO will be able to read the Avery Dennison RF700048 HF tag, which uses the NXP ICODE SLIX chip.

Thanks,

Narek

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Dec 10, 2019 1:07 PM UTC

    Hi ,

    the ST25R3911B-DISCO Discovery kit for ST25R3911B can be operated as an ISO15693 reader thus the memory of the aforementioned tags can be read using the READ SINGLE BLOCK command as defined in ISO/IEC 15693-3.

    On PC side, you can use either the ST25R3911B Discovery GUI (STSW-ST25R001) or the ST25PC-NFC Windows® PC software (STSW-ST25PC001).

    Feel free to share more details about your application.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    1 reply

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Dec 10, 2019 1:07 PM UTC

    Hi ,

    the ST25R3911B-DISCO Discovery kit for ST25R3911B can be operated as an ISO15693 reader thus the memory of the aforementioned tags can be read using the READ SINGLE BLOCK command as defined in ISO/IEC 15693-3.

    On PC side, you can use either the ST25R3911B Discovery GUI (STSW-ST25R001) or the ST25PC-NFC Windows® PC software (STSW-ST25PC001).

    Feel free to share more details about your application.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.