Associate III
March 16, 2022
Solved
ST25R3911 using without a library
- 2 replies
- 1355 views
Can anyone suggest ,pls, what should be the sequence of the registers configuration for ST25R3911 as a 14443-A reader , and the mechanism for sending and receiving APDU commands. Taking into account that there is no possibility to use the library (not a STM controller is used in the project)
I am trying to analyze the dialogue between the ST25 and the controller on the ST25R3911B-DISCO board using log.analyzer (file in attachment) .
For example,the user manual for PN7150(NXP) have clear instructions in which register and what value should be written in order to send APDU. If something similar exists for ST - I'lll be glad for any hint .