Skip to main content
Marius Celliers
Associate III
February 8, 2018
Solved

ST25R3911 No Response After second APDU Command

Posted on February 08, 2018 at 14:54

Hi .. I am currently sending an APDU Command to a card with the ST25R3911 and get a valid response.

I use the HAL drivers and middleware from ST-CubeMX ( CPU = STM32F401RE)

As soon as I try to send another APDU command ( or even the same one again) I receive 0 bytes from the card.

I start With rfalIsoDepPollAHandleActivation()

   then i set up may parameters (rfalIsoDepApduTxRxParam)

   then I send my first APDU Command. (rfalIsoDepApduBufFormat)

  err = rfalIsoDepStartApduTransceive(myParam);

   then I wait for the response in a loop with rfalworker()

         

for (int i=0;i<TIMEOUT;i++)

            {

               // Run the RFAL Worker

               rfalWorker();

              err = rfalIsoDepGetApduTransceiveStatus(); //Check The Status of the APDU Transceive

               if (err == ERR_NONE)

               {

                     logUsart('APDU Transceive Success\r\n');

                     rfalWorker();

                     HAL_Delay(20);

                     break;

                 }

               HAL_Delay(20);

               if (err == ERR_BUSY)

               {

                  logUsart('.');

               }

            }

   

after I received my rxBuf data,

   I change the txBufLen  and apdu command and send the data to the card, but now i get 0 bytes returned.

   also if i send the same apdu command to the card I also get 0 bytes returned.

my first apdu sending code is exactly the same as the second apdu sending code.

I also clear my Rx and Tx APDU buffers before loading the next C-APDU.

   

   ST_MEMSET(&apduCommand.apdu,0x00,sizeof(apduCommand.apdu));

      ST_MEMSET(&apduResponse.apdu,0x00,sizeof(apduResponse.apdu));

Is there any other initialization or,  setting of parameters, that I am missing ?

I believe that I should not try to run 

rfalIsoDepPollAHandleActivation() again (before the next APDU Transceive) as I am not disconnecting the card in any way.

#send-apdu #nfc #st25r3911b #apdu
    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    February 9, 2018
    Posted on February 09, 2018 at 17:14

    Hi Marius,

    looks like the state machine of the driver is not advancing. Maybe an issue in the interrupt porting. Can you grab a multimeter and measure the INT pin of ST25R3911B? If it is high then the ISR is not exexuted. 

    Regards, Ulysses 

    4 replies

    Ulysses HERNIOSUS
    ST Technical Moderator
    February 9, 2018
    Posted on February 09, 2018 at 14:40

    Hi Marius,

    yes, you should not try to reactivate the card. 

    Not sure what is happening but a few ideas for more information:

    • I assume you feed in the parameters received during activation (rfalIsoDepDevice->DID,FWT,dFWT and FsX) into the rfalIsoDepApduTxRxParam ? 
    • What is the value of your err variable - when it is neither ERR_None nor ERR_Busy?
    • The Hal_Delay(20) is too large, if the received APDU is larger then some 90+x bytes then this will overflow the FIFO of ST25R3911B

    Regards, Ulysses

    Marius Celliers
    Associate III
    February 9, 2018
    Posted on February 09, 2018 at 15:26

    HI Ulysses

    Thank you for your reply.

    Yes, After Activation I use the parameters returned from tfalIsoDepDevice

    err =

    rfalIsoDepPollAHandleActivation(RFAL_COMPLIANCE_MODE_NFC_11,RFAL_ISODEP_FSXI_512,RFAL_ISODEP_NO_DID,RFAL_BR_424,

    &isoDepDevice

    );

    myParam.DID = RFAL_ISODEP_NO_DID;     

    //isoDepDevice.info.DID; //

    myParam.FWT = isoDepDevice.info.FWT;

    myParam.dFWT = isoDepDevice.info.dFWT;

    myParam.FSx = isoDepDevice.info.FSx;

    myParam.ourFSx = RFAL_ISODEP_FSX_KEEP ;

    myParam.txBuf = &apduCommand;

    myParam.txBufLen = apduTxLen;

    myParam.rxBufLen = &apduRxLen;

    myParam.rxBuf = &apduResponse;

    On Sending a Second APDU to the Card :

    I get No error when I transmit err = rfalIsoDepStartApduTransceive(myParam);

    I Use a 'for' routine that runs ( 35 times.  I later changed it to 350 times) to get the Transceive status.

    So after 350 times calling the rfalWorker(); and rfalIsoDepGetApduTransceiveStatus();

    I still get ERR_BUSY after the 350 cycles. ( My response for the second APDU Command should be more or the same size as the first apdu command that I have sent)

    I have changed my loop with a delay of HAL_Delay(1) and retries of 2000 ( TIMEOUT = 2000)

    for (int i=0;i<TIMEOUT;i++)

    {

             

         

        err = rfalIsoDepGetApduTransceiveStatus();

    //Check The Status of the APDU Transceive

             HAL_Delay(1);

             

    // Run the RFAL Worker

             rfalWorker();

             if (err == ERR_NONE)

             {

                      logUsart('APDU Transceive Success\r\n');

                      rfalWorker();

                      HAL_Delay(1);

                      break;

               }

             HAL_Delay(1);

             if (err == ERR_BUSY)

             {

                     

    //  logUsart('.');

             }

    } 

    // for loop end

    logUsart('AID Receive Buffer have %d Bytes\r\n',apduRxLen);

    if (apduRxLen > 0)

    {

          logUsart('Rx Data: %s\r\n',hex2Str(apduResponse.apdu,apduRxLen));

    }

    Just to be sure, I have written the all parameters again in the Param struct before sending the second APDU comand.

    myParam.txBuf = &apduCommand;// &apduCommand;

    myParam.txBufLen = apduTxLen;

    myParam.rxBufLen = &apduRxLen;

    myParam.rxBuf = &apduResponse;

    myParam.DID = RFAL_ISODEP_NO_DID;//isoDepDevice.info.DID; //

    myParam.FWT = isoDepDevice.info.FWT;

    myParam.dFWT = isoDepDevice.info.dFWT;

    myParam.FSx = isoDepDevice.info.FSx;

    myParam.ourFSx = RFAL_ISODEP_FSX_KEEP ;

    but still no response on the second apdu command, ( also,I removed the USART Write command from ERR_BUSY in case of timing issues)  but stays on ERR_BUSY.

    Ulysses HERNIOSUS
    ST Technical Moderator
    February 9, 2018
    Posted on February 09, 2018 at 17:14

    Hi Marius,

    looks like the state machine of the driver is not advancing. Maybe an issue in the interrupt porting. Can you grab a multimeter and measure the INT pin of ST25R3911B? If it is high then the ISR is not exexuted. 

    Regards, Ulysses