Visitor II
July 2, 2018
Solved
ST25DVxxx V_EH output voltage
- 1 reply
- 1080 views
Posted on July 02, 2018 at 11:04
Hi
I'm playing around with an ST25DV_Discovery_ANT_C6 and an ST25R3911B-DISCO development board to test the energy harvesting features. One result of my tests yields, that the output voltage V_EH is limitted to approx. 3.4V eventhough I can't find any explenation therefore in any application note or datasheet.
R = 10kOhm
In the datasheet of the ST25DVxxx is written, that the voltage V_EH is NOT regulated. If that's true, I'm not able to understand my measurements.
Do you have any explenation for this behavior?
Thanks and best regards
Marco
energy-harvesting st25dv64k st25r3911b-disco