Skip to main content
Associate III
October 6, 2025
Solved

ST25dv64KC: how to use Fast Extended Read Multiple Blocks?

I'm using ST25dv64KC memory and need to use Fast Extended Read Multiple Blocks C5h, but I haven't had any success.

I'm passing the sequence "22C502E00251678F057ABB000001F00"

22 - request flags
C5 - Fast Extended Read Multiple Blocks
02 - IC mfg code
XXXXXXXXXXXXXXX - my UID
0000 - starting block
1F00 - ending block

This topic has been closed for replies.
JL. Lebon
JL. LebonBest answer
ST Employee
October 6, 2025

Hello, 

The Fast commands use a doubled data-rate for the tag-to-reader transmission.
This doubled data-rate is not supported by smartphones as of today. Only RFID readers can receive double data-rate responses.
So, if you are using a smartphone, you will not be able to use the Fast commands.
if you are using a RFID reader, you must inform the reader to listen for a double data-rate answer, otherwise it will not understand the answer.

Best regards.

5 replies

Andrew Neil
Super User
October 6, 2025

Have you established basic comms with the memory?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
GreidimarAuthor
Associate III
October 6, 2025

I already read and write to the ST25dv64KC memory using Extended Read Single Block - 30h and Extended Write Single Block - 31h.

I enter the memory password and then read.

But I want to make it faster, and the Fast Extended Read Multiple Blocks - C5h command doesn't work.

I use the Flutter NFC Kit library.

JL. Lebon
JL. LebonBest answer
ST Employee
October 6, 2025

Hello, 

The Fast commands use a doubled data-rate for the tag-to-reader transmission.
This doubled data-rate is not supported by smartphones as of today. Only RFID readers can receive double data-rate responses.
So, if you are using a smartphone, you will not be able to use the Fast commands.
if you are using a RFID reader, you must inform the reader to listen for a double data-rate answer, otherwise it will not understand the answer.

Best regards.

GreidimarAuthor
Associate III
October 6, 2025

I use Android and iPhone smartphones so it won't work?

JL. Lebon
ST Employee
October 6, 2025

Yes, unfortunately it is not supported by Android phones and iPhones. Only standard high data-rate is supported by those (26kb/s). You can use the Extended read multiple blocks command but not the Fast extended read multiple blocks command.

Best regards.