Skip to main content
Associate II
February 27, 2026
Solved

ST25DV64K - Embedded software

Hi

We are developing a product based on the ST25DV-I2C TAG.
I noticed that the X-CUBE-NFC4 software module is NRD. Can you suggest any software module that we could use to speed up development?
I also tried porting the existing FTM application from ST25NFC_Embedded_Lib_ST25R3911B_1.8.0. I found it very difficult to extract the FTM protocol from this library due to the enormous amount of dependencies. Do you also have a more appropriate FTM sample code to port to our application?

BR

Gilberto

This topic has been closed for replies.
Cedric Dalban
Cedric DalbanBest answer
ST Employee
March 3, 2026

Hello Gilberto,

The X-CUBE-NFC4 software module is now indeed NRD, you can use the package X-CUBE-NFC7 which replaces it.

Concerning your porting concern, feel free to have a look to the STSW-ST25DV002 or the STSW-ST25DV009 packages that are both also using the FTM library.
They provide some code example easing the porting of FTM protocol.

Last point, you can find some few documentation on st.com related to the FTM:
- AN5512: details the FTM component APIs
- UM2949: details the FTM protocol
- UM3078: details the use of FTM component on Linux

- UM2062: details the FTM low-level protocol + FTM Light protocol (see Annex A)

Best regards,
Cedric.

1 reply

Cedric Dalban
Cedric DalbanBest answer
ST Employee
March 3, 2026

Hello Gilberto,

The X-CUBE-NFC4 software module is now indeed NRD, you can use the package X-CUBE-NFC7 which replaces it.

Concerning your porting concern, feel free to have a look to the STSW-ST25DV002 or the STSW-ST25DV009 packages that are both also using the FTM library.
They provide some code example easing the porting of FTM protocol.

Last point, you can find some few documentation on st.com related to the FTM:
- AN5512: details the FTM component APIs
- UM2949: details the FTM protocol
- UM3078: details the use of FTM component on Linux

- UM2062: details the FTM low-level protocol + FTM Light protocol (see Annex A)

Best regards,
Cedric.