Skip to main content
Associate III
January 31, 2024
Solved

ST25 SDK for .NET

  • January 31, 2024
  • 5 replies
  • 2015 views

Is there a .NET SDK for ST25 NFC tags that will let me read and write ISO 15693 Type 5 tags in C#? I have the ST25R3911B-DISCO reader/writer board.

The closest I've found so far is a COMMS dll which appears to be taken from the demo app and will not load under 64-bit .NET. I've also seen the Java SDK but that looks like it is using the same DLL under the covers and is again 32-bit only, so I can't use it in my 64-bit app.

I would ideally like to be able to use these tags from a modern (.net 8 64-bit) app. Any suggestions appreciated.

This topic has been closed for replies.
Best answer by NFC/RFID Customer support

Hello,

just to inform that 64-bit version (3.0.0) is now available on STMicroelectronics web site: STSW-ST25PC001

NFCRFIDCustomersupport_0-1712754366346.png

ST25PC001: windows application & ST25PC002: source codes. DLLs are avaible after application install in install folder ./app/ or ST25PC002: resources/x64/

Best regards,

NFC Customer support

5 replies

ST Employee
February 16, 2024

Unfortunately, there is no plan to deliver a 64bits version of the 3911B dll for the moment.

You can eventually switch to ST25R3916B-DISCO  version that has a 64 bits version 

TimLongAuthor
Associate III
February 22, 2024

Having obtained the ST25R3916B unit and downloaded the software package, I still can't seem to find a 64-bit DLL. It looks like there is only a 32-bit version still. Are you certain this model has 64-bit support? Where can I find the DLL? The source code refers to "ST25R3916DISCOComm_x64.dll" which doesn't seem to be included in the download.

Best regards,

Tim Long

Tesla DeLorean
Guru
February 16, 2024

Perhaps look to the .NET community?

GHI Electronics always seemed to have a .NET focus 

https://www.ghielectronics.com/

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NFC/RFID Customer support
ST Employee
March 22, 2024

Hello

a new release of ST25-NFC software (STSW-ST25PC001) is planned for Wk14-2024. This new revision will be built in 64-bit version. After software install, you will be able to find all 64-bit DLL in the install directory/app, including ST25R3916DISCOComm.dll. Please, have a look on STMicroelectronics internet web site to get this new release soon.

Best regards,

NFC Customer Support

NFC/RFID Customer support
ST Employee
April 10, 2024

Hello,

just to inform that 64-bit version (3.0.0) is now available on STMicroelectronics web site: STSW-ST25PC001

NFCRFIDCustomersupport_0-1712754366346.png

ST25PC001: windows application & ST25PC002: source codes. DLLs are avaible after application install in install folder ./app/ or ST25PC002: resources/x64/

Best regards,

NFC Customer support