Skip to main content
Associate
October 27, 2025
Solved

Software Development Kit for ST25 Tags and Dynamic Tags - Android integration

  • October 27, 2025
  • 3 replies
  • 372 views

Hello,

I hope this is not a duplicate but I didn't find a similar issue.

I'm developing for my company an Android app using the STSW-ST25SDK001 - Software Development Kit for ST25 Tags and Dynamic Tags (https://www.st.com/en/embedded-software/stsw-st25sdk001.html).

To use your SDK i have to include two artifacts:

  • st25sdk-1.13.0.jar
  • st25_android_reader_interface-1.0.12-release.aar, specific for Android

I see that the AAR includes an "application" tag in its AndroidManifest.xml, even if it's only a library and does not provide an Application class:

<application
android:allowBackup="true"
android:label="@string/app_name"
android:supportsRtl="true" >
</application>

This cause Gradle to complain and fail build with the following error:

 

Manifest merger failed : Attribute application@allowBackup value=(false) from AndroidManifest.xml:7:9-36
is also present at [st25_android_reader_interface-1.0.12-release.aar] AndroidManifest.xml:10:9-35 value=(true).
Suggestion: add 'tools:replace="android:allowBackup"' to <application> element at AndroidManifest.xml:5:5-50:19 to override.
 
We can use "tools:replace" in our app manifest but it seems more of a workaround which makes the app build but sometimes still replaces the correct configuration as described here https://stackoverflow.com/a/36626818/3853058
 
I think the "application" part in the AAR Manifest should be removed, is it possible please?
 
Thanks
Best answer by France Berthelot

Hello 

Thanks for the highlight, we will handle this on next release (probably mid of december)

BR

FB

 

 

3 replies

NickVimarAuthor
Associate
November 3, 2025

hell @all any feedback on this?

Explorer II
November 13, 2025

Hi! I’ve encountered the same manifest declaration. It’s not critical, but a cleaner AAR without the application tag would definitely help. Following this discussion for updates.

France Berthelot
France BerthelotBest answer
ST Employee
November 25, 2025

Hello 

Thanks for the highlight, we will handle this on next release (probably mid of december)

BR

FB