Skip to main content
Associate II
February 2, 2026
Solved

RFAL Infinite Loop While Checking for Interrupt - ST25R3911b

Hi,

 

I have been working on a project that is based on the ST25R3911b Discovery Board including building prototype firmware from the discovery kit's firmware. I have made sure not to edit any of the RFAL or HAL library files.

Recently I had brought this prototype to be pre-scanned for radiated immunity. During this testing, I discovered a bug that I have not seen before.

The process gets stuck in an infinite loop in the rfalTransceiveRunBlockingTx() function (found in rfal_st25r3911b.c).
Specifically on line 1267, while( (rfalIsTransceiveInTx() && (ret == ERR_BUSY)) );

In the rfalTransceiveTx() function, the process enters the RFAL_TXRX_STATE_TX_WAIT_TXE case and checks for interrupts. However, there will not be any interrupts to process, and so the process breaks without updating the gRFAL.TxRx.state.
This appears to me like the interrupt from the NFC chip was either not sent or was not received correctly, so when that Do while loop checks "(ret == ERR_BUSY)", it will always be busy because the no interrupts are received and the state isn't changed.

It looks like a sanity timer was added in newer versions of RFAL, but I am mainly interested to know if this issue was seen before. It is unclear to me whether or not this could potentially be a hardware issue or if it's just firmware.

 

Some extra notes:

The system works most of the time, so I am confident that an additional system is not causing the problem.
The problem is intermittent and I have no way to consistently reproduce it. 

I can step out of the loop just fine and things work properly from there on.

 

Would anyone be able to shed some light on this?

 

Thank you,

Kaitlyn

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
February 9, 2026

Hi Kaitlyn,

I think the problem is the Calibrate Antenna which your software seems to issue asynchronously. The sequence towards the end is triggering sending an NFCV frame and then without waiting for I_txe, I_rxs/I_rxe/I_nre triggering the calibrate command. Such sequence is likely voiding the transmit and then software waits forever on I_txe. 

The calibrate function should only be called synchronously while there is no ongoing transmit/reception.

Typically it is sufficient to call it only once at startup. Only if you are targeting changing environment you can try calling it once in a while.

BR, Ulysses

7 replies

Brian TIDAL
ST Technical Moderator
February 3, 2026

Hi,

could you provide the RFAL version being used (see RFAL_VERSION in rfal_rf.h)?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ulysses HERNIOSUS
ST Technical Moderator
February 3, 2026

Hi Kaitlyn,

  1. the sanity timer is specifically meant to catching missing receive interrupts which could be happening under mentioned conditions.
  2. I am expecting a missing I_txe only in case the tx_en=0. To my knowledge software is checking this before triggering a transmit. Could you do a logic analyzer trace of the is behavior and share it here. Also interesting would be a dump of all the registers of ST25R3911B when this hang has happened.

BR, Ulysses

KRauccioAuthor
Associate II
February 5, 2026

Hi,

I apologize for the delayed response. I am struggling to reproduce the issue after setting up a logic analyzer. I will add an update later when I am able to provide the data.

I did get a chance to test a unit that was not used for immunity testing and I see the same issue there, so I doubt that those tests caused any issue.

 

@Brian TIDAL The RFAL version is stated to be v2.0.2. The RFAL files were ported from the ST25R3911b firmware.

 

 

Ulysses HERNIOSUS
ST Technical Moderator
February 6, 2026

Hi,

RFAL v2.0.2 is rather old but looking through the ReleaseNotes from latest v4.0.0 I didn't spot any bugs being fixed which sound like you are encountering. You could try to update to latest RFAL and see if it gets fixed. But my hopes are limited and for sure some APIs have changed since then.

Best to analyze based on a trace.

Ulysses