Skip to main content
Senior
April 23, 2020
Solved

RFAL_ANALOG_CONFIG for ST25R3916

I made a PCB with ST25R3916. And now is coding for it. The only example I can find is X-CUBE-NFC6. Because my usage of ST25R3916 has some differences with the NFC061A. For example, I don't need AAT and only use a fixed external attena (is it possible, right?) So, my analog configuration shouldn't be the same with NFC061A, right? I think I should do some changes with 'analogConifgTbl_NFC061A.c'. So, are there any docs about the usage of the RFAL analog config macros?

Update:

In AN5309, it states:

In the RFAL, these settings are referred to as analog configs/settings and the library applies them as needed. These settings are conveniently grouped in a table that can be easily customized and generated using available tools. 

Are there some tools to help?

Best regards.

    This topic has been closed for replies.
    Ulysses HERNIOSUS
    ST Technical Moderator
    April 23, 2020

    Hi,

    please have a look at ST25R3916-DISCO GUI: There you will find an "Analog Config" tab which allows you to load, store, r/w write from/to board analog configs in an convenient manner. It is even able to generate the aforementioned analogConfigTbl_NFC06A1.c.

    Regards, Ulysses

    1 reply

    Ulysses HERNIOSUS
    ST Technical Moderator
    April 23, 2020

    Hi,

    please have a look at ST25R3916-DISCO GUI: There you will find an "Analog Config" tab which allows you to load, store, r/w write from/to board analog configs in an convenient manner. It is even able to generate the aforementioned analogConfigTbl_NFC06A1.c.

    Regards, Ulysses