Skip to main content
Gaston
Associate III
December 23, 2020
Solved

reading/writing N213 tags using rfal

Hi,

How can I easily write/read N213 tags using rfal v2.2.0?

For the v1.3.2 version I used to call rfalISO14443ATransceiveFrame() to do it but I don't know how it's done in this latest stack version.

regards,

gaston

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
December 23, 2020

Hi Gaston,

you can use the functions in rfal_t2t.c. Depending on your needs you can also use the NDEF layer used e.g. in STSW-ST25R-LIB or X-CUBE-NFC6 to read/write NDEF on formatted tags.

Regards, Ulysses

3 replies

Ulysses HERNIOSUS
ST Technical Moderator
December 23, 2020

Hi Gaston,

you can use the functions in rfal_t2t.c. Depending on your needs you can also use the NDEF layer used e.g. in STSW-ST25R-LIB or X-CUBE-NFC6 to read/write NDEF on formatted tags.

Regards, Ulysses

Gaston
GastonAuthor
Associate III
December 24, 2020

Thanks Ulysses, it was just what I wanted and the write / read functions work as expected.

Besides, I also have to implement a password authentication (read) access but I see in the library that it is only available for NFC-V (ISO15693) tag families. Would an implementation of a password protection be available for T2T?

regards,

gaston

Gaston
GastonAuthor
Associate III
December 29, 2020

Hi Ulysses,

Currently I see that there is no password authentication implementation in rfal_t2t. Therefore I have added my own function that works correctly and that I have no problem to share it.

/*******************************************************************************/
 ReturnCode rfalT2TPollerAuth( uint32_t pwd, uint8_t* rxBuf, uint16_t rxBufLen, uint16_t *rcvLen )
 {
 ReturnCode ret;
 rfalT2TAuthReq req;
 
 if( (rxBuf == NULL) || (rcvLen == NULL) )
 {
 return ERR_PARAM;
 }
 
 req.code = (uint8_t)RFAL_T2T_CMD_PWD_AUTH;
 req.pwd[0] = pwd;
 req.pwd[1] = pwd>>8;
 req.pwd[2] = pwd>>16;
 req.pwd[3] = pwd>>24;
 
 /* Transceive Command */
 ret = rfalTransceiveBlockingTxRx( (uint8_t*)&req, sizeof(rfalT2TAuthReq), rxBuf, rxBufLen, rcvLen, RFAL_TXRX_FLAGS_DEFAULT, RFAL_FDT_POLL_READ_MAX );
 
 /* T2T 1.0 5.2.1.7 The Reader/Writer SHALL treat a NACK in response to a READ Command as a Protocol Error */
 if( (ret == ERR_INCOMPLETE_BYTE) && (*rcvLen == RFAL_T2T_ACK_NACK_LEN) && ((*rxBuf & RFAL_T2T_ACK_MASK) != RFAL_T2T_ACK) )
 {
 return ERR_PROTO;
 }
 return ret;
 }

You should call

rfalT2TPollerAuth(password, rfidRxBuf, 2, &rcvLen); 

and expect 2 bytes of PACK in rfidRxBuf

regards,

gaston