Skip to main content
Associate II
May 14, 2025
Solved

Questions about ST25 NFC Reader’s Tag Read Speed and Multi-Tag Handling

Hi,

I’m exploring the ​ST25 NFC Reader for a ​bio-tracking application that requires ​fast tag read speeds and reliable ​multi-tag detection. However, I couldn’t find detailed specifications in the datasheet regarding these aspects.

I’ve also purchased the ​STEVAL-ST25R200SA kit, but its provided GUI doesn’t seem to support tag read speed evaluation. Could you help clarify:

  1. ​Tag Read Speed:

    • What is the approximate ​read speed (tags/second) for the ST25 series (e.g., ST25R3916B)?
    • Is there a document (e.g., application note or performance report) that quantifies this?
  2. ​Evaluation Tools:

    • Are there other ​ST evaluation boards (e.g., X-NUCLEO-NFC08A1) that include tools to measure read speed?
  3. ​Multi-Tag Considerations:

    • When multiple tags are present in the ​ROI (e.g., 5 tags), what factors should I consider?
    • For example, could ​tag-to-tag coupling cause interference?

Context:

  • Tags: Small ​ISO/IEC 15693 glass tubes (2mm × 12mm).

Thanks in advance for your insights!

This topic has been closed for replies.
mike-johnBest answer
Visitor II
May 14, 2025

I ran into similar limitations when evaluating ST’s NFC readers for a multi-tag application. The GUI tools are great for basic tests but fall short for benchmarking real-time performance. You might want to dig into ST’s application notes—especially those around ISO 15693 anti-collision and multi-tag reading. Also, switching to something like the X-NUCLEO-NFC08A1 with a custom firmware approach gave us more flexibility in measuring read speeds and handling interference.

6 replies

mike-johnBest answer
Visitor II
May 14, 2025

I ran into similar limitations when evaluating ST’s NFC readers for a multi-tag application. The GUI tools are great for basic tests but fall short for benchmarking real-time performance. You might want to dig into ST’s application notes—especially those around ISO 15693 anti-collision and multi-tag reading. Also, switching to something like the X-NUCLEO-NFC08A1 with a custom firmware approach gave us more flexibility in measuring read speeds and handling interference.

StarryLiuAuthor
Associate II
May 14, 2025

Thanks for sharing your experience! I think I’ll eventually switch to the ​X-NUCLEO-NFC08A1 since it offers more flexibility for development.

By the way, in your experience, what’s the approximate ​read speed achievable with this setup? I’m targeting around ​50 reads per second—is that feasible with ISO 15693 tags?

Brian TIDAL
ST Technical Moderator
May 14, 2025

Hi,

can you elaborate on "What is the approximate ​read speed (tags/second) for the ST25 series"? Do you mean Inventory of the various ISO15693 tags in the operating field (i.e. retrieve the UID of each tag) or Inventory + reading of the tag memory content?

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
StarryLiuAuthor
Associate II
May 14, 2025

Thanks for the clarification! Yes, I specifically meant the inventory speed (tags/second) for ISO/IEC 15693 tags in the operating field—not including memory read operations.

Brian TIDAL
ST Technical Moderator
May 14, 2025

Hi,

the typical NFC Forum collision resolution process includes a 1-slot Inventory followed by a 16-slot Inventory in case of collision has been detected during the 1-slot Inventory. Further 16-slot Inventory commands may follow when further collisions are detected.

Here a typical sequence with 5 tags in the field of a ST25R3916B reader:

invent16.png

In dark blue, the Inventory Requests and in light blue the Inventory Responses. The 1st command is a 1-slot Inventory followed by collisions (5 tags replying). The 2nd command is a 16-slot Inventory followed by 5 answers in slots 1, 5, 7, 8 and 9 without collision. 

So basically the inventory speed is not reader dependent. Without collision during the 16-slot Inventory, one can expect to detect 5 tags in ~90ms if one of the tags replies in the last slot. In case of collision, further inventory commands are needed.

Hope this clarifies.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
StarryLiuAuthor
Associate II
May 15, 2025

Thanks for the details! The 90ms for 5 tags speed should work perfectly for my needs. Really helpful to know that inventory speed isn't reader-dependent.