Skip to main content
Visitor II
November 19, 2024
Solved

Problems with P2P connection (st25r3911b-disco)

Hello everyone,
I'm trying to establish a stable p2p connection between two st25r3911b disco boards. I'm still figuring things out and using the demo code as a reference to get it working.
I get one communication, but after that I break out of my while loop.
ReturnCode11 -> protocol error.

Kind regards
T_shower

 

void P2Pcommunication( rfalNfcDevice *nfcDev )
{
#if RFAL_FEATURE_NFC_DEP

 uint16_t *rxLen;
 uint8_t *rxData;
 ReturnCode err;

 if( nfcDev->type == RFAL_NFC_POLL_TYPE_AP2P )
 {
 	TransceiveBlocking( NULL, 0, &rxData, &rxLen, RFAL_FWT_NONE);
 }

 while(err == ERR_NONE)
 {
 	snprintf((char*)message,sizeof(message),message_stringsh);
 err = TransceiveBlocking( message, strlen(message), &rxData, &rxLen, RFAL_FWT_NONE);
 if( err != ERR_NONE )
 {
 break;
 }

 CDC_Transmit_FS(*rxData, sizeof(rxData) );
 }
#endif /* RFAL_FEATURE_NFC_DEP */
}

 

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
November 19, 2024

Hi,

not completely following how you perform this. Is this PC-Based using APIs of the firmware or is this directly in the firmware on STM32L4?

We do have a working example inside our STSW-ST25R-LIB: ap2p_proprietary which demonstrates based on firmware to exchange some data between two 3911,3916,3916B and derivates.

 

BR, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
November 19, 2024

Hi,

not completely following how you perform this. Is this PC-Based using APIs of the firmware or is this directly in the firmware on STM32L4?

We do have a working example inside our STSW-ST25R-LIB: ap2p_proprietary which demonstrates based on firmware to exchange some data between two 3911,3916,3916B and derivates.

 

BR, Ulysses