Skip to main content
Associate
January 3, 2024
Solved

Problem with st25dv16k ISO 15693 iOS communication

Hello!

I am trying to read some blocks from a iso 15693 tag. I can do it with Android without any problem. But when I try to do it with iOS I always receive the response [255,255]. What does it mean?

For example:

22 33 E0 02 51 00 02 4E BE 55 08 00 32 00 

Flags: 22

Function: 33 (Extended read multiple blocks)

Uid: E0 02 51 00 02 4E BE 55

Start block: 00 08

Number of blocks: 00 32

I don't know if the problem is the CRC16.

It occurs the same when I try to send the present password (B3 function), I receive the same response.

I know is not necessary to append it in Android, but, is it necessary in iOS?

which algorithm of CRC16 I have to use?

which bytes I have to use to generate CRC? all the message (22 33 E0 02 51 00 02 4E BE 55 08 00 32 00)? 

Thank you!

 

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
January 8, 2024

Hi,

rather than diving straight into more elaborate commands I would start off with a standard read single block.

I would be surprised if the CRC would be needed by iOS. I think you you should be able to inspect STSW-ST25IOS002 which should show you how to use iOS for your use cases.

 

BR, Ulysses

4 replies

Brian TIDAL
ST Technical Moderator
January 3, 2024

Hi,

The UID is transmitted least significant byte first. In your trace "22 33 E0 02 51 00 02 4E BE 55 08 00 32 00 " the UID is most significant byte first.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
koyAuthor
Associate
January 4, 2024

Hi!

I tried:
22 33 55 BE 4E 02 00 51 02 E0 08 00 32 00

22 33 55 BE 4E 02 00 51 02 E0 08 00 32 00 0E 7F

22 33 55 BE 4E 02 00 51 02 E0 08 00 32 00 7F E0

And the same code appears [255,255]. ¿what does that code mean?

thank you in advance

 

 

 

Ulysses HERNIOSUS
ST Technical Moderator
January 8, 2024

Hi,

rather than diving straight into more elaborate commands I would start off with a standard read single block.

I would be surprised if the CRC would be needed by iOS. I think you you should be able to inspect STSW-ST25IOS002 which should show you how to use iOS for your use cases.

 

BR, Ulysses