Skip to main content
Associate III
September 21, 2023
Solved

Problem with Bluetooth communication through ST25DV64KC-DISCO NFC module

Hey, for Bluetooth connection through the NFC tag I have given my Bluetooth mac address in the firmware code of the board, and now when I read the board through NFC-enabled mobile, it is pairing with my mobile, whose mac address is given into the firmware board, but it is not getting connected automatically. Can anyone help with this problem and give me a solution? I am also sharing a screen snippet of my firmware code.

Ndef_Bluetooth_OOB_t BleOOB = {.Type = NDEF_BLUETOOTH_BREDR,//standard bluetooth
 .DeviceAddress = NDEF_DEMO_BLE_ADDR_BIG_ENDIAN,//ble 
 mac address is given here 
 .DeviceAddressType = NDEF_BLE_PUBLIC_ADDRESS_TYPE,
 .Role = NDEF_BLE_ROLE_CENTRAL_ONLY ,
 .OptionalMask = 
 NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_COMPLETE_LOCAL_NAME),
 .LocalName = NDEF_DEMO_BLE_NAME, 
 };

void NDEF_DEMO_Read_Bluetooth_OOB(void)
{
 uint16_t status;
	sRecordInfo_t record;
 Ndef_Bluetooth_OOB_t bluetooth_oob;

 NDEF_DEMO_Init_Tag();

 status = getNDEFRecord(&record);
	if(status != NDEF_OK)
 {
		Menu_MsgStatus("Read OOB failure!","Cannot get the record!",MSG_STATUS_ERROR);
 return;
 }
 
 status = NDEF_ReadBluetoothOOB(&record,&bluetooth_oob);
 if(status != NDEF_OK)
 {
 Menu_MsgStatus("Read OOB failure!","OOB has not been read!",MSG_STATUS_ERROR);
	}
 else
 {
 /* 50 bytes for headers + data */////////////////////
 char *msg = (char *)malloc(50 +
 sizeof(bluetooth_oob.DeviceAddress) +
 strlen(bluetooth_oob.LocalName));
 if(msg == NULL)
 {
 Menu_MsgStatus("Memory error!","Cannot allocate memory",MSG_STATUS_ERROR);
 return;
 }
 
 strcpy(msg,"Type: ");
 if(bluetooth_oob.Type == NDEF_BLUETOOTH_BREDR)
 {
 strcat(msg,"BR/EDR\n\n");
 }
 else if (bluetooth_oob.Type == NDEF_BLUETOOTH_BLE)
 {
 strcat(msg,"BLE\n\n");
 } 
 strcat(msg,"DeviceAddress:\n");
 
 char device_address[18];
 sprintf(device_address, "%02X:%02X:%02X:%02X:%02X:%02X",bluetooth_oob.DeviceAddress[0],
 bluetooth_oob.DeviceAddress[1],
 bluetooth_oob.DeviceAddress[2],
 bluetooth_oob.DeviceAddress[3],
 bluetooth_oob.DeviceAddress[4],
 bluetooth_oob.DeviceAddress[5]);
 
 strcat(msg,device_address);
 strcat(msg,"\n\nLocal name:\n"); 
 strcat(msg,bluetooth_oob.LocalName);
 		Menu_MsgStatus("OOB content",msg,MSG_STATUS_SUCCESS);

 free (msg);
 
 } 
}
This topic has been closed for replies.
Rene Lenerve
Rene LenerveBest answer
ST Employee
October 10, 2023

Hi @PoolBear,

I think I was able to reproduce your issue with the device address buffer not set in the correct order.

Can you do a test by inverting data in the device address buffer to see if that fixes it.

Kind Regards.

1 reply

Rene Lenerve
Rene LenerveBest answer
ST Employee
October 10, 2023

Hi @PoolBear,

I think I was able to reproduce your issue with the device address buffer not set in the correct order.

Can you do a test by inverting data in the device address buffer to see if that fixes it.

Kind Regards.