Skip to main content
eoved
Visitor II
Mar 5, 2014 8:04 PM UTC
Solved

presence of multiple tags

Posted on March 05, 2014 at 21:04

Hi.

I am using CR95HF.

I need to identify the presence of multiple  iso15693 tags ( placed on the same time ).

I need to know how the amount of tags only.

Is ther a command or algorithm ?.

Please Advise.

Ephraim Oved

#cr95hf-iso15693 #m24lr #cr95hf #multi-tag #collision
This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Mar 6, 2014 12:08 PM UTC
Posted on March 06, 2014 at 13:08

Hello,

Are you using our software in order to control CR95HF?

The inventory algorithm 16 slots is implemented inside.

If not, inventory command is serving this aim; it is needed to control it. 

 In order to detect presence of many tags , it is needed to send an inventory 1 slot with a zero  masklength value.

If there is a collision

  • Start an  inventory  16 slots with masklength at value 0, so no maskvalue.
  • Many use cases possible for each slot 
    1.  No answer, go to next slot (send EOF only)
    2. Answer without any collision, recover UID
    3. Answer with collision, recover slot number Sni
    4. Complete or not the evaluation of the other slots
    5. Put in quiet the other already identified tags
    6. Start an inventory 16 slots with masklength = previous masklength+4 (0 + 4 from the first iteration) and maskvalue=previous maskvalue||SNi (Sni from first iteration)
    7. Recover first step
    8. If no more collision detected,end algo

Have a nice day,

Best regards,

ST NFC/RFID Dynamic tag online support

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Mar 6, 2014 12:08 PM UTC
Posted on March 06, 2014 at 13:08

Hello,

Are you using our software in order to control CR95HF?

The inventory algorithm 16 slots is implemented inside.

If not, inventory command is serving this aim; it is needed to control it. 

 In order to detect presence of many tags , it is needed to send an inventory 1 slot with a zero  masklength value.

If there is a collision

  • Start an  inventory  16 slots with masklength at value 0, so no maskvalue.
  • Many use cases possible for each slot 
    1.  No answer, go to next slot (send EOF only)
    2. Answer without any collision, recover UID
    3. Answer with collision, recover slot number Sni
    4. Complete or not the evaluation of the other slots
    5. Put in quiet the other already identified tags
    6. Start an inventory 16 slots with masklength = previous masklength+4 (0 + 4 from the first iteration) and maskvalue=previous maskvalue||SNi (Sni from first iteration)
    7. Recover first step
    8. If no more collision detected,end algo

Have a nice day,

Best regards,

ST NFC/RFID Dynamic tag online support