Skip to main content
Dnahm.1
Visitor II
October 1, 2020
Solved

peer to peer mode to 2-5 meters distance

We looking for a RFID devices (modules,IC) that can communicate in peer to peer mode to 2-5 meters distance (support anti collision algorithm) for iot implementation,

Please advise

This topic has been closed for replies.
Travis Palmer
Travis PalmerBest answer
ST Employee
October 1, 2020

Hello Dnahm.1,

NFC RFID is defined as proximity communication technology. In the books a communication range of several cm is mentioned, typically a range of 10cm is mentioned.

There are ISO15693 Reader available from reader makers which can communicate up to 1m range using 5w to 15W amplifier and additional filtering for the RX path.

You could have a look at UHF RFID which has a bigger operating area. The suitable product family would be the ST25RU.

BR Travis

1 reply

Travis Palmer
Travis PalmerBest answer
ST Employee
October 1, 2020

Hello Dnahm.1,

NFC RFID is defined as proximity communication technology. In the books a communication range of several cm is mentioned, typically a range of 10cm is mentioned.

There are ISO15693 Reader available from reader makers which can communicate up to 1m range using 5w to 15W amplifier and additional filtering for the RX path.

You could have a look at UHF RFID which has a bigger operating area. The suitable product family would be the ST25RU.

BR Travis