Skip to main content
calai
Visitor II
December 8, 2015
Solved

Number of NDEF files on ST25TA64K

Posted on December 08, 2015 at 01:22

The default configuration has 1 NDEF file that occupies the entire memory. Is it possible to slice up the memory between 2 or more NDEF files?  If more than one file can be created, what is the maximum number of files that on tag can accommodate? Is that 15 (inferred from SELECT command)?

#ndef-st25ta64k
    This topic has been closed for replies.
    Berenice BENVEGUDA
    ST Technical Moderator
    February 26, 2016
    Posted on February 26, 2016 at 10:57

    Dear Don,

     YOur understanding is correct. With ST25TA64K product you have to use NDEF file structure, memory cannot be adressed directly.

    Best Regards,

    NFC Product support1

    3 replies

    Berenice BENVEGUDA
    ST Technical Moderator
    December 11, 2015
    Posted on December 11, 2015 at 15:13

    Dear Sibi,

    ST25TA64K supports only 1 NDEF file.

    Could I ask you for which application you need more than 1 NDEF file ?

    Could several NDEF records be used within the NDEF file in your case ?

    Best Regards,

    NFC Product support1

    dsnedigar
    Visitor II
    February 23, 2016
    Posted on February 23, 2016 at 16:51

    Is it possible to use the ST25TA64K as just memory, i.e. not used NDEF at all ?

    We need to store a small amount of binary data, but don't need NDEF.  However, I don't see anything in thge ST25XXX data sheets that indicate this is possible, and that use of NDEF is mandatory for this series of RFID tags.  Is this correct ?

    Berenice BENVEGUDA
    ST Technical Moderator
    February 26, 2016
    Posted on February 26, 2016 at 10:57

    Dear Don,

     YOur understanding is correct. With ST25TA64K product you have to use NDEF file structure, memory cannot be adressed directly.

    Best Regards,

    NFC Product support1