Skip to main content
Visitor II
September 9, 2025
Solved

Not able to read the ST25 tag

Hi everyone!

I am currently testing the reading of a tag with an ST25TV02K chip using two different readers. Both readers are based on the same NFC chip and use the same antenna coil, but they differ in the matching network between the NFC chip and the antenna.

In theory, the first reader should be better matched to the NFC chip, while the second reader should be less well matched (and therefore expected to deliver less power). I have verified the reader matching using a VNA. However, I am observing an issue: at the same tag-to-reader distance and with the same power settings, tag read/write operations with the ST25TV02K sometimes fail when using the better-matched reader. 

This makes me wonder whether the better-matched reader might actually be delivering too much power to the tag, such that the VAC0–VAC1 voltage exceeds the maximum limit, preventing the ST25TV02K from responding correctly. Conversely, the less well-matched reader could be delivering lower power, keeping VAC0–VAC1 within the allowed range, which results in stable tag reading.

Does anyone know if this interpretation makes sense? And if so, is there any documentation or reference material that explains this behavior in detail?


This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
September 9, 2025

Hi,

could also be that the better matched reader draws too much power and overloads its power supply. This might lead to noise and reception issues on the NFC reader chip.

I think you need to use a scope and debug to see where the issue is: Tag does not respond or Reader fails to decode the answer.

BR, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
September 9, 2025

Hi,

could also be that the better matched reader draws too much power and overloads its power supply. This might lead to noise and reception issues on the NFC reader chip.

I think you need to use a scope and debug to see where the issue is: Tag does not respond or Reader fails to decode the answer.

BR, Ulysses