Skip to main content
KKulk.1
Associate
Mar 23, 2022 4:30 AM UTC
Solved

NFC reader supporting ST25DV

In our project, we are using ST micro NFC chip (ST25DV). So, the query is which card Reader be supported to read/write data for ST micro NFC chip (ST25DV)? Secondly, which PC-based applications can be used to see the data after reading or writing

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Mar 23, 2022 8:36 AM UTC

    Hi,

    ST25R readers such as

    can be used to communicate with ST25DV Dynamic tags.

    For the PC based application, I would recommend to use the ST25PC-NFC Windows® PC software with either a Discovery kit for the ST25R3916 or with a Discovery kit for the ST25R3911B.

    The ST25PC-NFC application provides access to the various features of the ST25DV tags

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    KKulk.1
    KKulk.1Author
    Associate
    Mar 23, 2022 4:32 AM UTC

    In our project, we are using ST micro NFC chip (ST25DV). So, the query is which card Reader be supported to read/write data for ST micro NFC chip (ST25DV)? Secondly, which PC-based applications can be used to see the data after reading or writing purposes? PC based application is necessary to read/write the data.

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Mar 23, 2022 8:36 AM UTC

    Hi,

    ST25R readers such as

    can be used to communicate with ST25DV Dynamic tags.

    For the PC based application, I would recommend to use the ST25PC-NFC Windows® PC software with either a Discovery kit for the ST25R3916 or with a Discovery kit for the ST25R3911B.

    The ST25PC-NFC application provides access to the various features of the ST25DV tags

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.