Skip to main content
kinder228
Associate II
Aug 20, 2013 9:49 AM UTC
Solved

My reader can read/write the M24LR04 but not M24LR16

Posted on August 20, 2013 at 11:49

Hello,

I'm using an RFID reader (Feig LRM1002) with 2 different version of the M24LRXX chip :

-

M24LR04E

(ANT3-M24LR04E)

-

M24LR16E

(ANT1-M24LR16E and ANT2-M24LR16E)

A problem appear when I scan my tag :

When I send an

''Inventory'' command there are no problems, I can see both versions of the chip.

The problem appear when I send a

''Read or Write Multiple Blocks'' command. With the M24LR16E I have an error message : ''No Transponder In Reader Field'' (it works well with the M24LR04E).

I tried the ''Extended Adress Mode'' but it didn't change anything.

Do you know what the problem could be ?

For information I use the demo software provided by the reader manufacturer (Feig ISOStart).

I took some screenshot :

http://www.fasthigh.info/browse.php?u=S5wrRyW4EcB3in6R9EG5XeQXepSbASj67PsDOz97Sdsgbcnjt2B3cHjHxcD12hLJ5qQrvUJYBaXu3g3s&b=5

http://www.fasthigh.info/browse.php?u=S5wrRyW4Ecd3in6R9EG5XeQXepSbASj67PsDOz97Sdsgbcnjt2B3cHjHxcD12hLB46Mhs0VdAqDu3g3s&b=5

Thank you

m24lr04e m24r04e 2-bytes m24lr16e devkit-m24lr-a m24lr-read-write-problem m24lr16e m24lr04e high-density

This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Aug 23, 2013 6:55 AM UTC
Posted on August 23, 2013 at 08:55

Hello Bill,

Please find also an application note that might help you :

AN4054: Comparison of RF addressing modes of low-density and high-density ISO/IEC 15693 devices

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00048677.pdf

Have a nice day,

All the best,

ST NFC/RFID Dynamic tag  

5 replies

Anais GALLIGANI
Visitor II
Aug 21, 2013 9:31 AM UTC
Posted on August 21, 2013 at 11:31

Hello,

It is linked that the M24LR16E is a high density memory ans as such is featuring 2-byte address vs. 1 byte address for low density ISO 15693 products. That is a minor firmware upgrade.

In order to further help you, might you send me your email please?

Thanks a lot,

Have a nice day,

All the best,

ST NFC/RFID Dynamic support

kinder228
kinder228Author
Associate II
Aug 22, 2013 7:22 AM UTC
Posted on August 22, 2013 at 09:22

Ok, thank you. So I need to upgrade my reader firmware.

Anais GALLIGANI
Visitor II
Aug 22, 2013 8:12 AM UTC
Posted on August 22, 2013 at 10:12

Hi ,

I can send you contact from Feig if you need to upgrade the firmware of their reader.

And also a firmware that might be compatible with your reader. It need to be test.

For that , I need your contact email .

kinder228
kinder228Author
Associate II
Aug 22, 2013 9:41 AM UTC
Posted on August 22, 2013 at 11:41

Ok, I already have some contacts with Feig. I'll contact them myself.

Thanks a lot for the infos

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Aug 23, 2013 6:55 AM UTC
Posted on August 23, 2013 at 08:55

Hello Bill,

Please find also an application note that might help you :

AN4054: Comparison of RF addressing modes of low-density and high-density ISO/IEC 15693 devices

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00048677.pdf

Have a nice day,

All the best,

ST NFC/RFID Dynamic tag