Skip to main content
Mihaita Ivascu
Associate III
August 7, 2025
Solved

Multiple tags are not detected

Hello,

 

   I use st25r3916 driver and DemoCycle from X-Cube-NFC6 app but devCnt for discovery is never more than 1 even though I have 2 tags next to the antenna and devLimit is set to 3.

 Also I see state machine never goes to RFAL_NFC_STATE_POLL_SELECT

 

How can I further debug it?

 

Thanks,

     Mihai

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
August 20, 2025

Hi Mihai,

 

what are the two tags you are using? If NFC-A then chances are that one is stronger than the other and the weaker one is not recognized as a collision during AntiCollision. You could work-around this by using rfalNfcaPollerSleepFullCollisionResolution() instead of rfalNfcaPollerFullCollisionResolution().

 

BR, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
August 20, 2025

Hi Mihai,

 

what are the two tags you are using? If NFC-A then chances are that one is stronger than the other and the weaker one is not recognized as a collision during AntiCollision. You could work-around this by using rfalNfcaPollerSleepFullCollisionResolution() instead of rfalNfcaPollerFullCollisionResolution().

 

BR, Ulysses