Skip to main content
Associate III
May 31, 2024
Solved

Mifare Classic reading with st25r3916

Hi,

I am implementing the st25r3916 firmware to be used in my reader. I have taken the code of "X-NUCLEO NFC06A1".

To make the authentication, I am able to send the command 0x60 + block number; I receive the answer and I send the next message with the key and I receive an answer from the card with length 4 bytes, but I have the status of the reader  "RFAL_ERR_PAR". But when I check the received 4 bytes, they are the right ones. I am using the flags:RFAL_TXRX_FLAGS_CRC_TX_MANUAL|RFAL_TXRX_FLAGS_CRC_RX_KEEP|RFAL_TXRX_FLAGS_NFCIP1_OFF |RFAL_TXRX_FLAGS_AGC_ON|RFAL_TXRX_FLAGS_PAR_RX_REMV|RFAL_TXRX_FLAGS_PAR_TX_NONE|RFAL_TXRX_FLAGS_CRC_RX_MANUAL

In order to continue with the reading, I was ommiting this error, and I am sending the command 0x30 to read, with the encryption (I know this part is well done due I have it already running in the st25r3911), in this case I am using next flags:

RFAL_TXRX_FLAGS_CRC_TX_MANUAL | RFAL_TXRX_FLAGS_CRC_RX_KEEP | RFAL_TXRX_FLAGS_NFCIP1_OFF | RFAL_TXRX_FLAGS_AGC_ON | RFAL_TXRX_FLAGS_PAR_RX_KEEP | RFAL_TXRX_FLAGS_PAR_TX_NONE|RFAL_TXRX_FLAGS_CRC_RX_MANUAL

but I do not receive any answer from the card. In this case I need to send 36 bits, due the parity ones, and I do not know if I need to change something to be able to send them, or if maybe the error cames from the previous parity error.

thanks,

 

Sandra

This topic has been closed for replies.
Ulysses HERNIOSUS
ST Technical Moderator
June 3, 2024

Hello Sandra,

maybe this discussion helps you a bit more:

https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/nfc0541-read-mifare-classic-1k/m-p/255197

BR, Ulysses

5 replies

SG3Author
Associate III
May 31, 2024

I have been making some more tests changing the flags after sending the 0x60 0x01 (authenticate block 1) and after receive the first answer from the card, I have tried next options:

- RFAL_TXRX_FLAGS_CRC_TX_MANUAL|RFAL_TXRX_FLAGS_CRC_RX_KEEP|RFAL_TXRX_FLAGS_NFCIP1_OFF |RFAL_TXRX_FLAGS_AGC_ON|RFAL_TXRX_FLAGS_PAR_RX_KEEP|RFAL_TXRX_FLAGS_PAR_TX_NONE|RFAL_TXRX_FLAGS_CRC_RX_MANUAL Error I receive is 40, and the lenght is 5 bytes

- RFAL_TXRX_FLAGS_CRC_TX_MANUAL|RFAL_TXRX_FLAGS_CRC_RX_REMV|RFAL_TXRX_FLAGS_NFCIP1_OFF |RFAL_TXRX_FLAGS_AGC_ON|RFAL_TXRX_FLAGS_PAR_RX_KEEP|RFAL_TXRX_FLAGS_PAR_TX_NONE|RFAL_TXRX_FLAGS_CRC_RX_MANUAL Error I receive is 40, and the lenght is 3 bytes (I can imagine that this is because it is removing the 2 bytes of CRC)

 

-RFAL_TXRX_FLAGS_CRC_TX_MANUAL|RFAL_TXRX_FLAGS_CRC_RX_KEEP|RFAL_TXRX_FLAGS_NFCIP1_OFF |RFAL_TXRX_FLAGS_AGC_ON|RFAL_TXRX_FLAGS_PAR_RX_REMV|RFAL_TXRX_FLAGS_PAR_TX_NONE|RFAL_TXRX_FLAGS_CRC_RX_MANUAL Error I receive is 27 (parity) anf the length is 4 bytes which after doing the calculations are the right ones.

Thanks,

 

Sandra

Ulysses HERNIOSUS
ST Technical Moderator
June 3, 2024

Hi Sandra,

 

I think the first variant is about right one but you need to use non-blocking variant of the interface which offers a bit oriented interface (rfalStartTransceive). The returned error means incomplete byte as 9 bits per byte are being received. Please also see the discussion in e.g. https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/nfc0541-read-mifare-classic-1k/m-p/255197.

 

BR, Ulysses

SG3Author
Associate III
June 3, 2024

Hi Ulysses,

I have read the discussion you have sent me several times, even before asking you. And I have not find any clue.

What I can not understand is the follow:

To make authentication:

1st transaction reader to card: 0x60+block with parity and CRC  ->ok

Answer card to reader must be: 4 Bytes with parity and NO CRC  ->ok

 

2nd transaction reader to card: 8 bytes with NO parity and NO CRC ->ok

**Answer card to reader must be: 4 Bytes with NO parity and NO CRC ->NOK

**How can be that this answer when I put those flags (RFAL_TXRX_FLAGS_CRC_TX_MANUAL|RFAL_TXRX_FLAGS_CRC_RX_KEEP|RFAL_TXRX_FLAGS_NFCIP1_OFF |RFAL_TXRX_FLAGS_AGC_ON|RFAL_TXRX_FLAGS_PAR_RX_KEEP|RFAL_TXRX_FLAGS_PAR_TX_NONE|RFAL_TXRX_FLAGS_CRC_RX_MANUAL) I receive 5 bytes from the card? Is the firmware somehow adding the parity byte?

What do you mean with non-blocking variant of the interface which offers a bit oriented interface (rfalStartTransceive)?Thanks,

Sandra

 

SG3Author
Associate III
June 10, 2024

After reading dozen of times the thread, finally I arrived to the point that the problem was that I was trying to send 36 bits, but the code was converting to 5 bytes, and of course the card was not able to answer due it was not understanding the command.

Thanks!!